This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC256XB-BT-SP: cc2564

Expert 1435 points

Replies: 4

Views: 322

Part Number: CC256XB-BT-SP

Tool/software: Code Composer Studio

Dear All,

i was testing keyfobs application with msp430f5438 + CC2564 Bluetooth evm using android phone, when prog is dumped for keyrfobs from SDK the phone detect Bluetooth device but paring is not happening,  will the issue solves if we use iPhone 

4 Replies

  • Hi,

    Could you please share exact steps that you have used to setup the keyfob application?

    Best regards,
    Vihang
  • In reply to Vihang Parmar:

    i have imported project that is available in SDK package  on CCS V5 and build and Debugged it 

    coming to hardware i connected a jumper to RF3 that is provided along with CC2564 EVM kit and all other jumpers remained in default position.

    coming to IOS i have tested and facing same problem as that of android it is detecting but not getting paired 

    Regards,

    Hussain 

  • In reply to Mohammed Hussain:

    Hussain,

    Have you verified that the correct CC256x service-pack is defined in the BTPSVEND.c file? The CC256XMSPBTBLESW uses the service-pack for the first generation CC256x by default. If using the CC256xB device (i.e. CC256XQFNEM), the __SUPPORT_CC256XB_PATCH__ macro must be defined when compiling the application code.

    More info: processors.wiki.ti.com/.../CC256x_MSP430_TI_Bluetooth_Stack

    Best regards,
    Vihang
  • In reply to Vihang Parmar:

    I did that one but problem continues its not getting paired any other way to check sensor outputs via ble module  

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.