Part Number: CC2564
Tool/software: TI C/C++ Compiler
Hi:
I use the TI SPPdemo of CC2564B,Now I set the CC2564B terminal as the client and use the command SetPairability Mode 2 (Attempts to set the Pairability Mode of the Local Device to Secure Simple Pairing)。
First,At the "Client>" prompt, enter Inquiry. This will initiate the Inquiry process. Once it is complete,I will get a list of all discovered devices.and then find the index number of the device I need to connect to, and pass Issue a Open <index number> <server port number> command at the command prompt。
After SPP is opened, the CC2564B terminal will send a pairing command to the mobile phone (Android platform). After clicking on the pairing, it can pair with the mobile phone. Next, we need to connect with the mobile phone. I don't know how to operate it. How CC2564B terminal Sends Connection Request to Mobile Phone?