Tool/software: Code Composer Studio
I'm using another BLE transmitter than the aoa_sender with a slightly different AdvData structure. The first 3 bytes are flags and cannot be changed. The rest of the packet has the same format as the sender_aoa AoA AdvData (meaning first 3 bytes are flags but byte 4 is the length, byte 6,7 Texas ID, 8 pkt ID, 6 bytes of padding and 17 bytes of '1's). I'm unable to receive anything during the AoA Scan at the receiver due to the mismatch in the AdvData bytes. Is there a way I can modify the aoa_receiver code to match the company ID at AdvData byte 6,7 and Packet ID at AdvData byte 8 to trigger the AoA packet event in RF core?
Thank you!