Part Number: CC2652R
Hello,
What is the default state of an unused pin in cc2652 ?
Regards,
Shyam
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
According to
it describes:
13.5 Unused I/O Pins
By default, the I/O driver (output) and input buffer (input) are disabled (tri-state mode) at power on or
reset, and thus the I/O pin can safely be left unconnected (floating).
If the I/O pin is in a tri-state condition and connected to a node with a different voltage potential, a small
leakage current can go through the pin. The same applies to an I/O pin configured as input, where the pin
is connected to a voltage source (for example VDD/2). The input is then an undefined value of either
0 or 1.