Part Number: CC2640R2F
Other Parts Discussed in Thread: CC2640
Tool/software: TI-RTOS
I held a tesla coil close to my CC2640R2F board. The CC2640R2F stops working , it can't be recovered automatically , i have to power it up again.
I have used the watchdog, in the watchdog interrupt callback the HAL_SYSTEM_RESET() is called. But no watchdog reset occurs, or it has ever generated a watchdog reset, but the reset failed.
It looks like the CC2640 is in the state of HIB, because when I connect the TCK directly to VCC , the CC2640R2F will not enter the halt , and when the Tesla coil is close to it, it always resets normally.
What should I do to solve this problem, this halt state is unacceptable, I hope it can be reset normally and recovered automatically when the Tesla coil is close to it.