Hi I have problem as below
• Scenario: HID device with CC2640R2. CC2640R2 is always failed to reconnect with Mac and Android Host. But there is no issue with Windows 10 Host. For OK case, after reconnect, CC2640R2 will send HID Report to Host.
• Test Environment:
SDK: simplelink_cc2640r2_sdk_2_40_00_32
HW: CC2640R2 launchpad
• Test steps:
1. CC2640R2 connect, just works pairing & bonding with Host.
2. On Host, turn off Bluetooth.
3. On Host, turn on Bluetooth.
4. CC2640R2 try to reconnect, but always fail.
Host | Bluetooth | OS |
HID Function test |
Reconnect test |
Android phone | V4.2 | android 7.0/ android 8.0 | PASS | FAIL |
Windows notebook | V5.0 | windows10 Professional ver1809 | PASS | PASS |
Windows notebook | V5.0 | windows10 Professional ver1803 | PASS | PASS |
Macbook | V4.0 | MacOS High Sierra | PASS | FAIL |
• Device log: CC2640R2 got GAPBOND_PAIRING_STATE BONED SUCCESS. But for GATT_Notification, the return value is blepending (0x16)
• Sniff log: Attach two logs
mac os sniffer : NG case.
Windows sniffer : OK case.
Below left snapshot is with MAC (NG case), right is with Windows10 (OK case). I find for the left, the encryption process is always fail.