Part Number: BOOSTXL-AOA
Other Parts Discussed in Thread: SIMPLELINK-CC2640R2-SDK
Hello,
I have some questions about the performance of Angle of Arrival BoosterPack(BOOSTXL-AOA).
1) How many degrees is the resolution of angle detection?
2) How long is the range of detection in meters?
3) It is indicated "The AoA angle error graph (the difference between the true angle on the incoming signal (phi) and the measured AoA). "
in the following page;
Can the above performance be achieveb by SIMPLELINK-CC2640R2-SDK.
4) It is indicated "A balanced signal is created using a marchand balun that is integrated in the PCB. " in the following page;
Please let me know how the ciucuit diagram and patturn shape of marchand balun.
5) I have watched the demo of Angle of Arrival BoosterPack of SIMPLELINK-CC2640R2-SDK.
But it seems that sampling rate is too slow(About 500ms?).
Can I accelerate the sampling rate?
Please advise.
Shoko