This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2650STK: CC2650STK

Part Number: CC2650STK
Other Parts Discussed in Thread: CC2650

Hello,

I'm trying to receive the signal of CC2650STK using a SDR (set as a receiver).

I'm configuring my SDR with the following parameters in order to receive signals:

1.  rf_channel=ISM2_4

2. rx_synthesizer_frequency=2.44 GHz (BLE)

3.  rf_rx_bandwidth=22 MHz

I was wondering with those parameters I would be able to catch the signals of CC2650 with my receiver

Thanks,

Mahsa

  • Hi Masha,

    For SDR related questions, this is not really the right place. 

    From your settings, I can at least see that the Rx BW will only cover a part of the 2.4 GHz band. As such, you will not be able to receive all packets sent by the SensorTag.

    Regards,
    Fredrik