This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

CC2650STK: CC2650STK

Prodigy 10 points

Replies: 1

Views: 91

Part Number: CC2650STK

Hello,

I'm trying to receive the signal of CC2650STK using a SDR (set as a receiver).

I'm configuring my SDR with the following parameters in order to receive signals:

1.  rf_channel=ISM2_4

2. rx_synthesizer_frequency=2.44 GHz (BLE)

3.  rf_rx_bandwidth=22 MHz

I was wondering with those parameters I would be able to catch the signals of CC2650 with my receiver

Thanks,

Mahsa

  • Guru 106355 points

    Hi Masha,

    For SDR related questions, this is not really the right place. 

    From your settings, I can at least see that the Rx BW will only cover a part of the 2.4 GHz band. As such, you will not be able to receive all packets sent by the SensorTag.

    Regards,
    Fredrik

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.