Hi ,
We have the CC2564MODA on our board and it started working (Logger file attached), We are working in UART cp3Wire mode, Currently we are stuck at the HCI_Reset function (int BTPSAPI HCI_Reset(unsigned int BluetoothStackID, Byte_t *StatusResult) file HCI.c, returning BTPS_ERROR_DEVICE_RESET_ERROR; we have started checking why we are getting the error and it looks as the flag HCI_CONTEXT_FLAGS_SYNCHRONOUS_HCI_FLAG is not set when we check it in the function HCISendPacket,
Any idea why this is happening maybe we are not setting/initialize some flags?
Please let me know if any other info. is needed,
Many Thanks
Loger Text
106 2 05/30/19 10:44:23.061 +0:00:00.000 BT Logger 1 uart_hci parameters: UartDIV=4, OS=17, SP=63, MoB=7
107 2 05/30/19 10:44:23.061 +0:00:00.000 BT Logger 1 temperature sensing: temp 26, read 0x20, vbe 0x2873319, slope 0x1f829
108 2 05/30/19 10:44:23.076 +0:00:00.015 BT Logger 1 Temperature region = 6
109 3 05/30/19 10:44:23.076 +0:00:00.015 BT Logger 1 In lc_rf_init_periodic_calibration
110 5 05/30/19 10:44:23.076 +0:00:00.015 BT Logger 1 synch event REG received, module RF_CALIBRATION, msi 0
111 5 05/30/19 10:44:23.076 +0:00:00.015 BT Logger 1 synch cmd start instance, module RF_CALIBRATION, msi: 0
112 5 05/30/19 10:44:23.076 +0:00:00.015 BT Logger 1 synch cmd return event STARTED,module RF_CALIBRATION
113 2 05/30/19 10:44:23.076 +0:00:00.015 BT Logger 1 ORCA Platform
114 2 05/30/19 10:44:23.076 +0:00:00.015 BT Logger 1 Process type: Nominal
115 2 05/30/19 10:44:23.076 +0:00:00.015 BT Logger 1 Chip revision: 6
116 2 05/30/19 10:44:23.076 +0:00:00.015 BT Logger 1 Detected Clock = 38400000 Hz
117 2 05/30/19 10:44:23.076 +0:00:00.015 BT Logger 1 Ref Clock = 38400000 Hz
118 2 05/30/19 10:44:23.076 +0:00:00.015 BT Logger 1 XTAL wakeup mode is disabled
119 2 05/30/19 10:44:23.076 +0:00:00.015 BT Logger 1 Ref Clock is valid for PLL
120 2 05/30/19 10:44:23.076 +0:00:00.015 BT Logger 1 PLL Clock Output is OK
121 2 05/30/19 10:44:23.076 +0:00:00.015 BT Logger 1 PLL Clock Out = 40000000 Hz
122 2 05/30/19 10:44:23.076 +0:00:00.015 BT Logger 1 Clock Working mode: PLL Mode
123 2 05/30/19 10:44:23.076 +0:00:00.015 BT Logger 1 ARM Clock = 40000000 Hz, Slow Clock: External
124 2 05/30/19 10:44:23.076 +0:00:00.015 BT Logger 1 OCP Clock = 8000000 Hz
125 4 05/30/19 10:44:23.076 +0:00:00.015 BT Logger 1 UART HCI baudrate = 116363
126 2 05/30/19 10:44:23.076 +0:00:00.015 BT Logger 1 Gemini type Soft Gemini
127 3 05/30/19 10:44:23.076 +0:00:00.015 BT Logger 1 lm_lc_get_local_features
128 3 05/30/19 10:44:23.076 +0:00:00.015 BT Logger 1 lm_lc_set_brcst_retran
129 3 05/30/19 10:44:23.076 +0:00:00.015 BT Logger 1 lm_lc_self_test_run_init_tests
130 2 05/30/19 10:44:23.076 +0:00:00.015 BT Logger 1 Self Test passed
131 4 05/30/19 10:44:23.076 +0:00:00.015 BT Logger 1 I2C doesn't exist !
132 3 05/30/19 10:44:23.076 +0:00:00.015 BT Logger 1 lm_lc_get_local_bd_addr
133 3 05/30/19 10:44:23.076 +0:00:00.015 BT Logger 1 Software version - 7.0.16
134 2 05/30/19 10:44:23.076 +0:00:00.015 BT Logger 1 Deactivating timer: init
135 3 05/30/19 10:44:23.076 +0:00:00.015 BT Logger 1 lm_lc_rf_periodic_calibration
136 2 05/30/19 10:44:23.076 +0:00:00.015 BT Logger 1 Calibration started. Vector=0x1, 0x0
137 2 05/30/19 10:44:23.076 +0:00:00.015 BT Logger 1 PHY FW Version 3.27
138 2 05/30/19 10:44:23.076 +0:00:00.015 BT Logger 1 random 0x0 0x9a1f
139 2 05/30/19 10:44:23.076 +0:00:00.015 BT Logger 1 random 0x2746 0x95b4
140 2 05/30/19 10:44:23.076 +0:00:00.015 BT Logger 1 random 0x98f9 0xf55
141 2 05/30/19 10:44:23.076 +0:00:00.015 BT Logger 1 random 0x7116 0x3be0
142 2 05/30/19 10:44:23.076 +0:00:00.015 BT Logger 1 random 0xa7e5 0xae71
143 3 05/30/19 10:44:23.076 +0:00:00.015 BT Logger 1 lm_lc_generate_rand
144 3 05/30/19 10:44:23.076 +0:00:00.015 BT Logger 1 lm_lc_generate_rand
145 5 05/30/19 10:44:23.076 +0:00:00.015 BT Logger 1 synch event FINISH received, module RF_CALIBRATION, msi 0
146 3 05/30/19 10:44:23.076 +0:00:00.015 BT Logger 1 lm_lc_generate_rand
147 3 05/30/19 10:44:23.076 +0:00:00.015 BT Logger 1 lm_lc_generate_rand
148 4 05/30/19 10:44:25.931 +0:00:02.870 BT Logger 1 Transport detection: UART detected
149 3 05/30/19 10:44:25.931 +0:00:02.870 BT Logger 1 first byte recevied C0
150 3 05/30/19 10:44:25.931 +0:00:02.870 BT Logger 1 Disable FLIGHT MODE - Enable TX calibration
151 4 05/30/19 10:44:25.931 +0:00:02.870 BT Logger 1 Uart Active Protocol: H5 PROTOCOL
152 4 05/30/19 10:44:50.782 +0:00:27.721 BT Logger 1 H5 RX, Receive msg SYNC
153 4 05/30/19 10:44:50.782 +0:00:27.721 BT Logger 1 H5 TX, send msg SYNC_RESPONSE
154 4 05/30/19 10:44:50.782 +0:00:27.721 BT Logger 1 H5 TX, send msg SYNC
155 7 05/30/19 10:44:51.203 +0:00:28.142 BT Logger 1 *** WARNING *** H5 TX, retransmit lc_msg
156 4 05/30/19 10:44:51.203 +0:00:28.142 BT Logger 1 H5 TX, send msg SYNC
157 7 05/30/19 10:44:51.609 +0:00:28.548 BT Logger 1 *** WARNING *** H5 TX, retransmit lc_msg
158 4 05/30/19 10:44:51.609 +0:00:28.548 BT Logger 1 H5 TX, send msg SYNC