Other Parts Discussed in Thread: CC2650, BLE-STACK
Tool/software: TI-RTOS
Hi all
I would like to implement data length extension in these two project. And I have taken throughput example as my reference.
But when I connect cc2650 to an ipad , everything is well. It means I am sure it do the mtu_exchange with IPAD , but not do so with
cc2650lanchpad(host_test) .
environment setting is [
compiler version is TI v18.1.4.LTS
code composer version is 8.2
SDK of ble is ble_sdk_2_02_02_25,
tirtos_cc13xx_cc26xx_2_21_01_08
]
When I want to exchangeMTU (GATT_EXCHANGE_MTU)by btool, it would end up MSG_BUFFER_NOT_AVAIL.
If I don't do any operation with btool. it would disconnect 7 seconds later after connection establishing.
It ends up the situation like the following screenshot.
any idea to figure out what happen?