Other Parts Discussed in Thread: BLE-STACK
Hi,
I am using CC2541 module for my application. I have attached sniffer log for one of the advertising device which is based on SimpleBLEPeripheral application. This capture is from the mobile whone connecting to CC2541 module.I am using different 3rd party android application for scanning and connecting the devices. I have multiple phones. I find that my actual device which is based on CC2541 module(running SIMPLEBLEPeripheral application) is not listed in some of the mobile app scanner. The same mobile in which CC2541 is failing to get scanned, is able to scan different other BLE devices(some of them are ibeacon also). This proves that BLE is supported on the phone in which CC2541 is failing to get scanned. My question is why the same module is being scanned and connected as well in some of the mobile phones but doesn't in some of them? Out of 5 mobiles, it is able to get scanned in just 2 devices. I have around 10 units of prototypes(only one powered at a time) with same CC2541 module and behavior is same with all modules with different 3rd party android app available on google play store. In sniffer, the CC2541 module shows advertising but not listed in some of the mobile phones
Regards
Narendra