Dear team,
In the antenna switching mode, a total of 32 switchings were made.
#define AOA_ANT_SWITCH_START_TIME 576 (12uS)
When AOA_ANT_SWITCH_START_TIME,is it always uses antenna 2? Or 12uS (antenna 2) plus 4uS initial antenna time (antenna 2), that is, the first 16uS antenna is antenna 2?
In addition, when three antennas are used, the antenna 2 is the initial antenna, and then the antenna is switched to the antenna 1, and then cyclically cycles through 10 cycles in the order of 1, 2, and 3, and then switches to the end of the antenna 2.
Am i right?