Part Number: CC1352R
Hello,
Currently I am trying to use sscanf() to parse a string of a little under 1000 bytes.
The code is as follows:
uint32_t socket = 0;
uint32_t length = 0;
char result[2048];
// Scan for the socket number (0 - 6) and message
if (sscanf(input, "+TEXT: %1u,%4u,\"%1023[^\"]", &socket, &length, result) != 3)
{
etc...
However, this does not work. The system hangs. When I reduce the 1023 bytes for the result string to 267 bytes, it works.
What might cause this? Inspecting the system with the ROV does not show a stack overflow.
Thanks for any insight!