I have installed "Smart RF Sniffer Agent - v1.6.0" on my windows system. On launching the software, I am getting "Autostart waring No devices are running as expected" error message.
Please guide how to resolve this issue.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have installed "Smart RF Sniffer Agent - v1.6.0" on my windows system. On launching the software, I am getting "Autostart waring No devices are running as expected" error message.
Please guide how to resolve this issue.
Hi,
When Sniffer Agent is launched with Auto Start enabled it will automatically start all connected sniffer devices. This can be used for example for automation purposes, so you can start up all from the command line. The warning you see is to tell that there is no sniffer devices connected to start.
You can disable Auto Start from the 'options' menu on the top of the GUI. There is a bug in Sniffer Agent that makes the GUI minimize too much and hide the menu bar when launched with Auto Start, so you might have to use the scrollbar to the right to be able to access it. This bug will be fixed in the version (1.8.0) that will be released in Mid January 2020.
Regards,
Bjørn