Part Number: CC1352P
Could you help in confirming if the changes in the values of component seen on the 2.4GHz and 900MHz Balun used on the latest Launchpad design files are crucial.
We had based our product design on an older version of the launchpad design files(shown below).
But on the latest launchpad design schematic I noticed these changes shown below:-
In addition the SWRA629A– Application Report for the Integrated Filter Balun for CC1352 shows the same design that we have initially incorporated.
Kindly help us confirm if we need to include the modifications as per the latest launchpad design or if we can continue with the current design we have. This is really urgent.