Part Number: TPS61093
Hi
Im using TPS61093DSKR as a booster from 3.7V to 6.5V.
the steady state current is about 15mA and every 5ms the current is ~70mA, the problem is the the Vout of the booster drops.
The design do not have 0.1uf on the VO , can it explain the problem? Can I shortcut VO and OUT?