Other Parts Discussed in Thread: SYSCONFIG
Tool/software: TI C/C++ Compiler
Team,
I got an inquiry about sample program of SimpleLink CC13x2_26x2 SDK from my customer. Customer is suffering from the HardFault exception in sample project - . Simple Broadcast. I have tried to build the simple broadcast sample and tried to do debug. It appears the program exit reached with HardFault exception as below:
///////////////////////////////
Mon Jan 20, 2020 13:21:46: Program exit reached.
Mon Jan 20, 2020 13:21:46: EXIT 0
Mon Jan 20, 2020 13:21:46: HardFault exception.
Mon Jan 20, 2020 13:21:46: The processor has escalated a configurable-priority exception to HardFault.
Mon Jan 20, 2020 13:21:46: A precise data access error has occurred (CFSR.PRECISERR, BFAR) at data address 0x20014048.
Mon Jan 20, 2020 13:21:46:
Mon Jan 20, 2020 13:21:46: Exception occured at PC = 0xffffffff, LR = 0x0
Mon Jan 20, 2020 13:21:46:
Mon Jan 20, 2020 13:21:46: See the call stack for more information.
Mon Jan 20, 2020 13:21:46: The stack pointer for stack 'CSTACK' (currently 0x20003430) is outside the stack range (0x20013C00 to 0x20014000)
///////////////////////////////
This phenomenon would be appeared in case of using the IAR-EW. The CCS does not have any problem. It also happen on both SDK3.30 and SDK3.40.
Could I have your comment on this?
Regards,
Nonaka