Hi,
We try to update advertising packets periodically and we wanted to use HCI_EXT_AdvEventNoticeCmd command to achieve it. After we added the command to the code we got
unresolved symbol HCI_EXT_AdvEventNoticeCmd, first referenced in <whole-program>
error. HCI_EXT_AdvEventNoticeCmd exists in included hci.h header file as
extern hciStatus_t HCI_EXT_AdvEventNoticeCmd( uint8 taskID, uint16 taskEvent );
but it goes nowhere when we try to open declaration. We checked icall_ble_api.h header file and there is either no HCI_EXT_AdvEventNoticeCmd or HCI_EXT_ConnEventNoticeCmd defined. We use the latest SimpleLink CC13X2 CC26X2 SDK 3_40_00_02. Is there any other similar commands?
Regards