Other Parts Discussed in Thread: CC2640R2F, CC2640, CC1350, CC1310, CC2650, SYSCONFIG
Note: The following instructions have been written for SDK 3_40_00_02 but can be adapted to quite any SDK version (that is why I provided the sources but also the diff files). In addition, the code was written for CC2642R but can be adapted to all the devices of the family (CC2652R, CC2652P, CC1352R, CC1352P). Even better, as the instructions deal with TI drivers only, they are valid for ALL the devices in the SimpleLink family (CC2640R2F, CC1310, CC1350, CC2640, CC2650).
In order to have easy-to-use and portable code, the TI drivers handle a lot of different configurations. Most of the time, a specific application does not require to handle all those configurations. By optimizing the TI drivers for your own application you can save FLASH and processor time.
A good example of this is the Power driver (but you can analyze any TI driver in order to optimize by following the same type of guidance).
The Power driver is a pretty generic driver. A lot of different combinations of crystals can be used and it handles all of them.
Let’s see how to optimize the Power driver.
1) Force CCS to not use the compiled sources for the Power driver. To do right click on your project and click “Add Files…”. Add the files PowerCC26X2.c and PowerCC26X2.h to your project.
I recommend to select Copy Files and not Link to files.
Verify if the compiler is considering the files you added by checking the “MODULE SUMMARY” section of the .map file. You should find the following line:
PowerCC26X2.obj 2102 84 272
2) Know the crystal configuration of your project:
- For CC26402: consult ccfg.c
- For CC26x2: consult SysConfig and/or ti_devices_config.c
3) Find code that will never be accessed knowing the configuration of the project. The best strategy is to look into the condition of the if statements. An always true (or always wrong) condition will allow deleting some code.
It is important to test properly your code in between the different optimizations!
- Do you use the VIMS RAM as GPRAM ?
-
-
- No, then CCFGRead_DIS_GPRAM() will always be true (or !CCFGRead_DIS_GPRAM() will always be false). Replace CCFGRead_DIS_GPRAM() by “true” or basically remove the corresponding if bloc.
-
- The source of the SCLK_LF is fixed. There is no point in using a function (CCFGRead_SCLK_LF_OPTION()) to read the source of the SCLK_LF every time. In the Power_init() function, the variable ccfgLfClkSrc can be replaced by a constant.
Here we can leverage the code optimizer. The useless code will basically not be generated!
- Have you enable a TCXO function? / Are you using the TCXO?
-
-
- No? Then (PowerCC26X2_config.enableTCXOFxn != NULL) and (CCFGRead_XOSC_FREQ() == CCFGREAD_XOSC_FREQ_TCXO) will always be false
-
In addition the function static void switchToTCXO(void) can be commented
- What did you chose as LF Clock Source?
The LF Clock Source is read using the following code: OSCClockSourceGet(OSC_SRC_CLK_LF). So every time this piece of code is called, we are going to replace it by a variable setting.
Here we can leverage the code optimizer. The useless code will basically not be generated!
- What did you chose as HF Clock Source?
Same procedure with the HF Clock Source
Replace the calls to OSCClockSourceGet(OSC_SRC_CLK_HF) by the value returned.
4) Finally we cut the Flash consumption of the file PowerCC26X2.c by almost 20%!
PowerCC26X2.obj 1686 84 272
Here are the diff and the modified files:
diff --git "a/C:\\ti\\simplelink_cc13x2_26x2_sdk_3_40_00_02\\source\\ti\\drivers\\power\\PowerCC26X2.c" "b/C:\\Users\\a0132664\\Documents\\WORK\\FLASH_OPTIMIZATION\\PowerDriver\\PowerCC26X2.c"
index fb30104..4b4771f 100644
--- "a/C:\\ti\\simplelink_cc13x2_26x2_sdk_3_40_00_02\\source\\ti\\drivers\\power\\PowerCC26X2.c"
+++ "b/C:\\Users\\a0132664\\Documents\\WORK\\FLASH_OPTIMIZATION\\PowerDriver\\PowerCC26X2.c"
@@ -78,7 +78,9 @@ static void disableLFClockQualifiers(void);
static void emptyClockFunc(uintptr_t arg);
static int_fast16_t notify(uint_fast16_t eventType);
static void oscillatorISR(uintptr_t arg);
-static void switchToTCXO(void);
+
+// CC_POWER_DRIVER_OPTIMIZATION - Have you enable a TCXO function? / Are you using the TCXO?
+//static void switchToTCXO(void);
/* RCOSC calibration functions functions */
extern void PowerCC26X2_calibrate(void);
@@ -250,7 +252,9 @@ void Power_idleFunc()
int_fast16_t Power_init()
{
ClockP_Params clockParams;
- uint32_t ccfgLfClkSrc;
+ // CC_POWER_DRIVER_OPTIMIZATION - constant source for SCLK_LF?
+ // uint32_t ccfgLfClkSrc;
+ const uint32_t ccfgLfClkSrc = CCFGREAD_SCLK_LF_OPTION_XOSC_LF;
/* CC26X2 PG1.0 trap. If we are running on PG1.0, spin forever.
* This hardware revision is no longer supported. This trap is
@@ -278,17 +282,18 @@ int_fast16_t Power_init()
/* Check if TCXO is selected in CCFG and in addition configured to be
* enabled by the function pointed to by PowerCC26X2_config.enableTCXOFxn
*/
- if ((CCFGRead_XOSC_FREQ() == CCFGREAD_XOSC_FREQ_TCXO) &&
- (PowerCC26X2_config.enableTCXOFxn != NULL)) {
-
- /* Construct the Clock object for TCXO startup time.
- * Set timeout to TCXO startup time as specified in CCFG.
- */
- ClockP_construct(&PowerCC26X2_module.tcxoEnableClock,
- (ClockP_Fxn)&switchToTCXO,
- (CCFGRead_TCXO_MAX_START()*100)/ClockP_tickPeriod,
- NULL);
- }
+// CC_POWER_DRIVER_OPTIMIZATION - Have you enable a TCXO function? / Are you using the TCXO?
+// if ((CCFGRead_XOSC_FREQ() == CCFGREAD_XOSC_FREQ_TCXO) &&
+// (PowerCC26X2_config.enableTCXOFxn != NULL)) {
+//
+// /* Construct the Clock object for TCXO startup time.
+// * Set timeout to TCXO startup time as specified in CCFG.
+// */
+// ClockP_construct(&PowerCC26X2_module.tcxoEnableClock,
+// (ClockP_Fxn)&switchToTCXO,
+// (CCFGRead_TCXO_MAX_START()*100)/ClockP_tickPeriod,
+// NULL);
+// }
/* construct the Clock object for scheduling of wakeups */
/* initiated and started by the power policy */
@@ -335,7 +340,8 @@ int_fast16_t Power_init()
DRIVERLIB_ASSERT_CURR_RELEASE();
/* read the LF clock source from CCFG */
- ccfgLfClkSrc = CCFGRead_SCLK_LF_OPTION();
+ // CC_POWER_DRIVER_OPTIMIZATION - constant source for SCLK_LF?
+ //ccfgLfClkSrc = CCFGRead_SCLK_LF_OPTION();
/* check if should calibrate RCOSC_LF */
if (PowerCC26X2_config.calibrateRCOSC_LF) {
@@ -394,10 +400,11 @@ int_fast16_t Power_init()
Power_setConstraint(PowerCC26XX_DISALLOW_STANDBY);
}
+//CC_POWER_DRIVER_OPTIMIZATION - Do you use the VIMS RAM as GPRAM?
/* if VIMS RAM is configured as GPRAM: set retention constraint */
- if (!CCFGRead_DIS_GPRAM()) {
- Power_setConstraint(PowerCC26XX_RETAIN_VIMS_CACHE_IN_STANDBY);
- }
+// if (!CCFGRead_DIS_GPRAM()) {
+// Power_setConstraint(PowerCC26XX_RETAIN_VIMS_CACHE_IN_STANDBY);
+// }
return (Power_SOK);
}
@@ -773,7 +780,8 @@ int_fast16_t Power_sleep(uint_fast16_t sleepState)
* the XOSC_HF "on" without having switched to is not
* considered by this driver.
*/
- if (OSCClockSourceGet(OSC_SRC_CLK_HF) == OSC_XOSC_HF ||
+ // CC_POWER_DRIVER_OPTIMIZATION - What did you chose as HF Clock Source? (here HF Clock Source is OSC_RCOSC_HF)
+ if (/*OSCClockSourceGet(OSC_SRC_CLK_HF)*/ OSC_RCOSC_HF == OSC_XOSC_HF ||
PowerCC26X2_module.xoscPending == true) {
xosc_hf_active = true;
configureXOSCHF(PowerCC26XX_DISABLE);
@@ -1120,7 +1128,9 @@ static void disableLFClockQualifiers(void)
uint32_t sourceLF;
/* query LF clock source */
- sourceLF = OSCClockSourceGet(OSC_SRC_CLK_LF);
+// CC_POWER_DRIVER_OPTIMIZATION - What did you chose as LF Clock Source? (here LF Clock Source is OSC_XOSC_LF)
+// sourceLF = OSCClockSourceGet(OSC_SRC_CLK_LF);
+ sourceLF = OSC_XOSC_LF;
/* is LF source either RCOSC_LF or XOSC_LF yet? */
if ((sourceLF == OSC_RCOSC_LF) || (sourceLF == OSC_XOSC_LF)) {
@@ -1276,42 +1286,46 @@ static unsigned int configureXOSCHF(unsigned int action)
* action more than once will not have any effect until the hardware triggers
* a software state change.
*/
+
+// CC_POWER_DRIVER_OPTIMIZATION - What did you chose as HF Clock Source? (here HF Clock Source is OSC_RCOSC_HF)
if (action == PowerCC26XX_ENABLE &&
- OSCClockSourceGet(OSC_SRC_CLK_HF) != OSC_XOSC_HF &&
+ /*OSCClockSourceGet(OSC_SRC_CLK_HF)*/ OSC_RCOSC_HF != OSC_XOSC_HF &&
PowerCC26X2_module.xoscPending == false) {
/* Check if TCXO is selected in CCFG and in addition configured to be enabled
* by the function pointed to by PowerCC26X2_config.enableTCXOFxn.
*/
- if ((CCFGRead_XOSC_FREQ() == CCFGREAD_XOSC_FREQ_TCXO) &&
- (PowerCC26X2_config.enableTCXOFxn != NULL)) {
-
- /* Enable power on TCXO */
- (*(PowerCC26X2_config.enableTCXOFxn))(true);
-
- /* Configure TCXO */
- HWREG(AUX_DDI0_OSC_BASE + DDI_O_CLR + DDI_0_OSC_O_CTL0) = DDI_0_OSC_CTL0_XTAL_IS_24M;
- HWREG(AUX_DDI0_OSC_BASE + DDI_O_SET + DDI_0_OSC_O_XOSCHFCTL) = DDI_0_OSC_XOSCHFCTL_BYPASS;
- if (CCFGRead_TCXO_TYPE() == 0x1)
- {
- /* Selected TCXO type is clipped-sine. Enabled internal common-mode bias. */
- HWREG( AUX_DDI0_OSC_BASE + DDI_O_SET + DDI_0_OSC_O_XOSCHFCTL ) = DDI_0_OSC_XOSCHFCTL_TCXO_MODE_XOSC_HF_EN;
- }
-
- /* Start clock to wait for TCXO startup time before clock switch
- * can be attempted.
- */
- ClockP_start(ClockP_handle(&PowerCC26X2_module.tcxoEnableClock));
- }
+// CC_POWER_DRIVER_OPTIMIZATION - Have you enable a TCXO function? / Are you using the TCXO?
+// if ((CCFGRead_XOSC_FREQ() == CCFGREAD_XOSC_FREQ_TCXO) &&
+// (PowerCC26X2_config.enableTCXOFxn != NULL)) {
+//
+// /* Enable power on TCXO */
+// (*(PowerCC26X2_config.enableTCXOFxn))(true);
+//
+// /* Configure TCXO */
+// HWREG(AUX_DDI0_OSC_BASE + DDI_O_CLR + DDI_0_OSC_O_CTL0) = DDI_0_OSC_CTL0_XTAL_IS_24M;
+// HWREG(AUX_DDI0_OSC_BASE + DDI_O_SET + DDI_0_OSC_O_XOSCHFCTL) = DDI_0_OSC_XOSCHFCTL_BYPASS;
+// if (CCFGRead_TCXO_TYPE() == 0x1)
+// {
+// /* Selected TCXO type is clipped-sine. Enabled internal common-mode bias. */
+// HWREG( AUX_DDI0_OSC_BASE + DDI_O_SET + DDI_0_OSC_O_XOSCHFCTL ) = DDI_0_OSC_XOSCHFCTL_TCXO_MODE_XOSC_HF_EN;
+// }
+//
+// /* Start clock to wait for TCXO startup time before clock switch
+// * can be attempted.
+// */
+// ClockP_start(ClockP_handle(&PowerCC26X2_module.tcxoEnableClock));
+// }
OSCHF_TurnOnXosc();
PowerCC26X2_module.xoscPending = true;
/* Unless it is disallowed, unmask the XOSC_HF ready to switch flag */
- if (!((CCFGRead_XOSC_FREQ() == CCFGREAD_XOSC_FREQ_TCXO) &&
- (PowerCC26X2_config.enableTCXOFxn != NULL)))
- {
+// CC_POWER_DRIVER_OPTIMIZATION - Have you enable a TCXO function? / Are you using the TCXO?
+// if (!((CCFGRead_XOSC_FREQ() == CCFGREAD_XOSC_FREQ_TCXO) &&
+// (PowerCC26X2_config.enableTCXOFxn != NULL)))
+// {
if (!(Power_getConstraintMask() & (1 << PowerCC26XX_SWITCH_XOSC_HF_MANUALLY))) {
/* Clearing the flag in the ISR does not always work. Clear it again just in case */
@@ -1320,7 +1334,7 @@ static unsigned int configureXOSCHF(unsigned int action)
/* Turn on oscillator interrupt for SCLK_HF switching */
HWREG(PRCM_BASE + PRCM_O_OSCIMSC) |= PRCM_OSCIMSC_HFSRCPENDIM_M;
}
- }
+// }
/* If the device goes into IDLE in between turning on XOSC_HF and
* and switching SCLK_HF to XOSC_HF, the INT_OSC_COMB HFSRCPEND
@@ -1336,21 +1350,22 @@ static unsigned int configureXOSCHF(unsigned int action)
OSCHF_SwitchToRcOscTurnOffXosc();
/* Handle TCXO if selected in CCFG */
- if (CCFGRead_XOSC_FREQ() == CCFGREAD_XOSC_FREQ_TCXO) {
-
- /* Turn off bias if clipped sine TCXO type */
- if (CCFGRead_TCXO_TYPE() == 1) {
- HWREG(AUX_DDI0_OSC_BASE + DDI_O_CLR + DDI_0_OSC_O_XOSCHFCTL) =
- DDI_0_OSC_XOSCHFCTL_TCXO_MODE_XOSC_HF_EN;
- }
-
- /* Check if function for enabling/disabling TCXO is supported */
- if (PowerCC26X2_config.enableTCXOFxn != NULL) {
-
- /* Disable TCXO by turning off power */
- (*(PowerCC26X2_config.enableTCXOFxn))(false);
- }
- }
+// CC_POWER_DRIVER_OPTIMIZATION - Have you enable a TCXO function? / Are you using the TCXO?
+// if (CCFGRead_XOSC_FREQ() == CCFGREAD_XOSC_FREQ_TCXO) {
+//
+// /* Turn off bias if clipped sine TCXO type */
+// if (CCFGRead_TCXO_TYPE() == 1) {
+// HWREG(AUX_DDI0_OSC_BASE + DDI_O_CLR + DDI_0_OSC_O_XOSCHFCTL) =
+// DDI_0_OSC_XOSCHFCTL_TCXO_MODE_XOSC_HF_EN;
+// }
+//
+// /* Check if function for enabling/disabling TCXO is supported */
+// if (PowerCC26X2_config.enableTCXOFxn != NULL) {
+//
+// /* Disable TCXO by turning off power */
+// (*(PowerCC26X2_config.enableTCXOFxn))(false);
+// }
+// }
/* If we have not actually switched to XOSC_HF yet, we need to
* undo what we did above when turning on XOSC_HF. Otherwise,
@@ -1377,12 +1392,13 @@ static unsigned int configureXOSCHF(unsigned int action)
* ======== switchToTCXO ========
* Switching to TCXO after TCXO startup time has expired.
*/
-static void switchToTCXO(void)
-{
- /* Enable clock qualification on 48MHz signal from TCXO */
- HWREG( AUX_DDI0_OSC_BASE + DDI_O_SET + DDI_0_OSC_O_XOSCHFCTL ) = DDI_0_OSC_XOSCHFCTL_TCXO_MODE;
-
- /* Switch to TCXO */
- switchXOSCHF();
-}
+// CC_POWER_DRIVER_OPTIMIZATION - Have you enable a TCXO function? / Are you using the TCXO?
+//static void switchToTCXO(void)
+//{
+// /* Enable clock qualification on 48MHz signal from TCXO */
+// HWREG( AUX_DDI0_OSC_BASE + DDI_O_SET + DDI_0_OSC_O_XOSCHFCTL ) = DDI_0_OSC_XOSCHFCTL_TCXO_MODE;
+//
+// /* Switch to TCXO */
+// switchXOSCHF();
+//}
/*
* Copyright (c) 2015-2019, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*/
/*
* ======== PowerCC26X2.c ========
*/
#include <stdbool.h>
#include <ti/drivers/dpl/HwiP.h>
#include <ti/drivers/dpl/ClockP.h>
#include <ti/drivers/dpl/SwiP.h>
#include <ti/drivers/dpl/DebugP.h>
#include <ti/drivers/Power.h>
#include <ti/drivers/power/PowerCC26X2.h>
/* driverlib header files */
#include <ti/devices/DeviceFamily.h>
#include DeviceFamily_constructPath(inc/hw_types.h)
#include DeviceFamily_constructPath(inc/hw_prcm.h)
#include DeviceFamily_constructPath(inc/hw_nvic.h)
#include DeviceFamily_constructPath(inc/hw_aux_sysif.h)
#include DeviceFamily_constructPath(inc/hw_aon_rtc.h)
#include DeviceFamily_constructPath(inc/hw_memmap.h)
#include DeviceFamily_constructPath(inc/hw_ccfg.h)
#include DeviceFamily_constructPath(inc/hw_rfc_pwr.h)
#include DeviceFamily_constructPath(inc/hw_aon_pmctl.h)
#include DeviceFamily_constructPath(inc/hw_fcfg1.h)
#include DeviceFamily_constructPath(inc/hw_ints.h)
#include DeviceFamily_constructPath(driverlib/sys_ctrl.h)
#include DeviceFamily_constructPath(driverlib/pwr_ctrl.h)
#include DeviceFamily_constructPath(driverlib/prcm.h)
#include DeviceFamily_constructPath(driverlib/aon_ioc.h)
#include DeviceFamily_constructPath(driverlib/aon_rtc.h)
#include DeviceFamily_constructPath(driverlib/aon_event.h)
#include DeviceFamily_constructPath(driverlib/osc.h)
#include DeviceFamily_constructPath(driverlib/cpu.h)
#include DeviceFamily_constructPath(driverlib/vims.h)
#include DeviceFamily_constructPath(driverlib/sys_ctrl.h)
#include DeviceFamily_constructPath(driverlib/driverlib_release.h)
#include DeviceFamily_constructPath(driverlib/setup.h)
#include DeviceFamily_constructPath(driverlib/ccfgread.h)
static unsigned int configureXOSCHF(unsigned int action);
static unsigned int nopResourceHandler(unsigned int action);
static unsigned int configureRFCoreClocks(unsigned int action);
static void switchXOSCHF(void);
static void disableLFClockQualifiers(void);
static void emptyClockFunc(uintptr_t arg);
static int_fast16_t notify(uint_fast16_t eventType);
static void oscillatorISR(uintptr_t arg);
// CC_POWER_DRIVER_OPTIMIZATION - Have you enable a TCXO function? / Are you using the TCXO?
//static void switchToTCXO(void);
/* RCOSC calibration functions functions */
extern void PowerCC26X2_calibrate(void);
extern bool PowerCC26X2_initiateCalibration(void);
extern void PowerCC26X2_auxISR(uintptr_t arg);
extern void PowerCC26X2_RCOSC_clockFunc(uintptr_t arg);
/* Externs */
extern const PowerCC26X2_Config PowerCC26X2_config;
/* Module_State */
PowerCC26X2_ModuleState PowerCC26X2_module = {
.notifyList = {0}, /* list of registered notifications */
.constraintMask = 0, /* the constraint mask */
.clockObj = {0}, /* Clock object for scheduling wakeups */
.calibrationClock = {0}, /* Clock object for RCOSC calibration */
.tcxoEnableClock = {0}, /* Clock object for TCXO startup */
.tdcHwi = {0}, /* hwi object for calibration */
.oscHwi = {0}, /* hwi object for oscillators */
.nDeltaFreqCurr = 0, /* RCOSC calibration variable */
.nCtrimCurr = 0, /* RCOSC calibration variable */
.nCtrimFractCurr = 0, /* RCOSC calibration variable */
.nCtrimNew = 0, /* RCOSC calibration variable */
.nCtrimFractNew = 0, /* RCOSC calibration variable */
.nRtrimNew = 0, /* RCOSC calibration variable */
.nRtrimCurr = 0, /* RCOSC calibration variable */
.nDeltaFreqNew = 0, /* RCOSC calibration variable */
.bRefine = false, /* RCOSC calibration variable */
.state = Power_ACTIVE, /* current transition state */
.xoscPending = false, /* is XOSC_HF activation in progress? */
.calLF = false, /* calibrate RCOSC_LF? */
.auxHwiState = 0, /* calibration AUX ISR state */
.busyCal = false, /* already busy calibrating */
.calStep = 0, /* current calibration step */
.firstLF = true, /* is this first LF calibration? */
.enablePolicy = false, /* default value is false */
.initialized = false, /* whether Power_init has been called */
.constraintCounts = { 0, 0, 0, 0, 0, 0, 0 },
.resourceCounts = { 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0 },
.resourceHandlers = {
configureRFCoreClocks,
configureXOSCHF,
nopResourceHandler
}, /* special resource handler functions */
.policyFxn = 0 /* power policyFxn */
};
/* resource database */
const PowerCC26XX_ResourceRecord resourceDB[PowerCC26X2_NUMRESOURCES] = {
{PowerCC26XX_PERIPH | PowerCC26XX_DOMAIN_PERIPH, PRCM_PERIPH_TIMER0}, /* PERIPH_GPT0 */
{PowerCC26XX_PERIPH | PowerCC26XX_DOMAIN_PERIPH, PRCM_PERIPH_TIMER1}, /* PERIPH_GPT1 */
{PowerCC26XX_PERIPH | PowerCC26XX_DOMAIN_PERIPH, PRCM_PERIPH_TIMER2}, /* PERIPH_GPT2 */
{PowerCC26XX_PERIPH | PowerCC26XX_DOMAIN_PERIPH, PRCM_PERIPH_TIMER3}, /* PERIPH_GPT3 */
{PowerCC26XX_PERIPH | PowerCC26XX_DOMAIN_SERIAL, PRCM_PERIPH_SSI0}, /* PERIPH_SSI0 */
{PowerCC26XX_PERIPH | PowerCC26XX_DOMAIN_PERIPH, PRCM_PERIPH_SSI1}, /* PERIPH_SSI1 */
{PowerCC26XX_PERIPH | PowerCC26XX_DOMAIN_SERIAL, PRCM_PERIPH_UART0}, /* PERIPH_UART0 */
{PowerCC26XX_PERIPH | PowerCC26XX_DOMAIN_SERIAL, PRCM_PERIPH_I2C0}, /* PERIPH_I2C0 */
{PowerCC26XX_PERIPH | PowerCC26XX_DOMAIN_PERIPH, PRCM_PERIPH_TRNG}, /* PERIPH_TRNG */
{PowerCC26XX_PERIPH | PowerCC26XX_DOMAIN_PERIPH, PRCM_PERIPH_GPIO}, /* PERIPH_GPIO */
{PowerCC26XX_PERIPH | PowerCC26XX_DOMAIN_PERIPH, PRCM_PERIPH_UDMA}, /* PERIPH_UDMA */
{PowerCC26XX_PERIPH | PowerCC26XX_DOMAIN_PERIPH, PRCM_PERIPH_CRYPTO}, /* PERIPH_CRYPTO */
{PowerCC26XX_PERIPH | PowerCC26XX_PERIPH_UDMA, PRCM_PERIPH_I2S}, /* PERIPH_I2S */
{PowerCC26XX_SPECIAL | PowerCC26XX_DOMAIN_RFCORE, 0}, /* PERIPH_RFCORE */
{PowerCC26XX_SPECIAL | PowerCC26XX_NOPARENT, 1}, /* XOSC_HF */
{PowerCC26XX_DOMAIN | PowerCC26XX_NOPARENT, PRCM_DOMAIN_PERIPH}, /* DOMAIN_PERIPH */
{PowerCC26XX_DOMAIN | PowerCC26XX_NOPARENT, PRCM_DOMAIN_SERIAL}, /* DOMAIN_SERIAL */
{PowerCC26XX_DOMAIN | PowerCC26XX_NOPARENT, PRCM_DOMAIN_RFCORE}, /* DOMAIN_RFCORE */
{PowerCC26XX_SPECIAL | PowerCC26XX_NOPARENT, 2}, /* DOMAIN_SYSBUS */
{PowerCC26XX_PERIPH | PowerCC26XX_DOMAIN_PERIPH, PRCM_PERIPH_PKA}, /* PERIPH_PKA */
{PowerCC26XX_PERIPH | PowerCC26XX_DOMAIN_PERIPH, PRCM_PERIPH_UART1}, /* PERIPH_UART1 */
};
/* ****************** Power APIs ******************** */
/*
* ======== Power_disablePolicy ========
* Do not run the configured policy
*/
bool Power_disablePolicy(void)
{
bool enablePolicy = PowerCC26X2_module.enablePolicy;
PowerCC26X2_module.enablePolicy = false;
return (enablePolicy);
}
/*
* ======== Power_enablePolicy ========
* Run the configured policy
*/
void Power_enablePolicy(void)
{
PowerCC26X2_module.enablePolicy = true;
}
/*
* ======== Power_getConstraintMask ========
* Get a bitmask indicating the constraints that have been registered with
* Power.
*/
uint_fast32_t Power_getConstraintMask(void)
{
return (PowerCC26X2_module.constraintMask);
}
/*
* ======== Power_getDependencyCount ========
* Get the count of dependencies that are currently declared upon a resource.
*/
int_fast16_t Power_getDependencyCount(uint_fast16_t resourceId)
{
DebugP_assert(resourceId < PowerCC26X2_NUMRESOURCES);
return ((int_fast16_t)PowerCC26X2_module.resourceCounts[resourceId]);
}
/*
* ======== Power_getTransitionLatency ========
* Get the transition latency for a sleep state. The latency is reported
* in units of microseconds.
*/
uint_fast32_t Power_getTransitionLatency(uint_fast16_t sleepState,
uint_fast16_t type)
{
uint32_t latency = 0;
if (type == Power_RESUME) {
if (sleepState == PowerCC26XX_STANDBY) {
latency = PowerCC26X2_RESUMETIMESTANDBY;
}
}
else {
if (sleepState == PowerCC26XX_STANDBY) {
latency = PowerCC26X2_TOTALTIMESTANDBY;
}
}
return (latency);
}
/*
* ======== Power_getTransitionState ========
* Get the current sleep transition state.
*/
uint_fast16_t Power_getTransitionState(void)
{
return (PowerCC26X2_module.state);
}
/*
* ======== Power_idleFunc ========
* Function needs to be plugged into the idle loop.
* It calls the configured policy function if the
* 'enablePolicy' flag is set.
*/
void Power_idleFunc()
{
if (PowerCC26X2_module.enablePolicy) {
if (PowerCC26X2_module.policyFxn != NULL) {
(*(PowerCC26X2_module.policyFxn))();
}
}
}
/*
* ======== Power_init ========
*/
int_fast16_t Power_init()
{
ClockP_Params clockParams;
// CC_POWER_DRIVER_OPTIMIZATION - constant source for SCLK_LF?
// uint32_t ccfgLfClkSrc;
const uint32_t ccfgLfClkSrc = CCFGREAD_SCLK_LF_OPTION_XOSC_LF;
/* CC26X2 PG1.0 trap. If we are running on PG1.0, spin forever.
* This hardware revision is no longer supported. This trap is
* provided to aid in automatically identifying PG1.0 devices
* in circulation and will be removed later in the year.
*/
if (!((HWREG(FCFG1_BASE + FCFG1_O_TFW_FT) % 10000) >= 683)) {
while (1);
}
/* if this function has already been called, just return */
if (PowerCC26X2_module.initialized) {
return (Power_SOK);
}
/* set module state field 'initialized' to true */
PowerCC26X2_module.initialized = true;
/* set the module state enablePolicy field */
PowerCC26X2_module.enablePolicy = PowerCC26X2_config.enablePolicy;
/* copy the Power policy function to module state */
PowerCC26X2_module.policyFxn = PowerCC26X2_config.policyFxn;
/* Check if TCXO is selected in CCFG and in addition configured to be
* enabled by the function pointed to by PowerCC26X2_config.enableTCXOFxn
*/
// CC_POWER_DRIVER_OPTIMIZATION - Have you enable a TCXO function? / Are you using the TCXO?
// if ((CCFGRead_XOSC_FREQ() == CCFGREAD_XOSC_FREQ_TCXO) &&
// (PowerCC26X2_config.enableTCXOFxn != NULL)) {
//
// /* Construct the Clock object for TCXO startup time.
// * Set timeout to TCXO startup time as specified in CCFG.
// */
// ClockP_construct(&PowerCC26X2_module.tcxoEnableClock,
// (ClockP_Fxn)&switchToTCXO,
// (CCFGRead_TCXO_MAX_START()*100)/ClockP_tickPeriod,
// NULL);
// }
/* construct the Clock object for scheduling of wakeups */
/* initiated and started by the power policy */
ClockP_Params_init(&clockParams);
clockParams.period = 0;
clockParams.startFlag = false;
clockParams.arg = 0;
ClockP_construct(&PowerCC26X2_module.clockObj,
&emptyClockFunc,
0,
&clockParams);
/*
* If RCOSC calibration is enabled, construct a Clock object for
* delays. Set timeout to 8 Clock tick periods to get
* ceil(8x10us/30.5us/SCLK_LF_period)*30.5us/SCLK_LF_period = ~90us.
* The total time we need to wait for AUX_SYSIF_TDCREFCLKCTL_ACK
* is about 105us and the ClockP_start() call needs about 21us.
* All together, that makes ~111us. A decent approximation of the
* ideal wait duration.
* In practice, the COMPARE_MARGIN that is currently still in
* the kernel Timer.c implementation may make it take longer
* than 90us to time out.
*/
ClockP_Params_init(&clockParams);
clockParams.period = 0;
clockParams.startFlag = false;
clockParams.arg = 0;
ClockP_construct(&PowerCC26X2_module.calibrationClock,
&PowerCC26X2_RCOSC_clockFunc,
8,
&clockParams);
HwiP_construct(&PowerCC26X2_module.oscHwi,
INT_OSC_COMB,
oscillatorISR, NULL);
HWREG(PRCM_BASE + PRCM_O_OSCIMSC) = 0;
/* construct the TDC hwi */
HwiP_construct(&PowerCC26X2_module.tdcHwi,
INT_AUX_COMB,
PowerCC26X2_auxISR, NULL);
DRIVERLIB_ASSERT_CURR_RELEASE();
/* read the LF clock source from CCFG */
// CC_POWER_DRIVER_OPTIMIZATION - constant source for SCLK_LF?
//ccfgLfClkSrc = CCFGRead_SCLK_LF_OPTION();
/* check if should calibrate RCOSC_LF */
if (PowerCC26X2_config.calibrateRCOSC_LF) {
/* verify RCOSC_LF is the LF clock source */
if (ccfgLfClkSrc == CCFGREAD_SCLK_LF_OPTION_RCOSC_LF) {
PowerCC26X2_module.calLF = true;
}
}
/*
* if LF source is RCOSC_LF or XOSC_LF: assert DISALLOW_STANDBY constraint
* and start a timeout to check for activation
*/
if ((ccfgLfClkSrc == CCFGREAD_SCLK_LF_OPTION_RCOSC_LF) ||
(ccfgLfClkSrc == CCFGREAD_SCLK_LF_OPTION_XOSC_LF)) {
/* Turn on oscillator interrupt for SCLK_LF switching */
HWREG(PRCM_BASE + PRCM_O_OSCIMSC) |= PRCM_OSCIMSC_LFSRCDONEIM_M;
/* disallow STANDBY pending LF clock quailifier disabling */
Power_setConstraint(PowerCC26XX_DISALLOW_STANDBY);
}
else if (ccfgLfClkSrc == CCFGREAD_SCLK_LF_OPTION_EXTERNAL_LF) {
/*
* else, if the LF clock source is external, can disable clock qualifiers
* now; no need to assert DISALLOW_STANDBY or start the Clock object
*/
/* yes, disable the LF clock qualifiers */
DDI16BitfieldWrite(
AUX_DDI0_OSC_BASE,
DDI_0_OSC_O_CTL0,
DDI_0_OSC_CTL0_BYPASS_XOSC_LF_CLK_QUAL_M|
DDI_0_OSC_CTL0_BYPASS_RCOSC_LF_CLK_QUAL_M,
DDI_0_OSC_CTL0_BYPASS_RCOSC_LF_CLK_QUAL_S,
0x3);
/* enable clock loss detection */
OSCClockLossEventEnable();
}
else if(ccfgLfClkSrc == CCFGREAD_SCLK_LF_OPTION_XOSC_HF_DLF) {
/* else, user has requested LF to be derived from XOSC_HF */
/* Turn on oscillator interrupt for SCLK_LF switching.
* When using HPOSC, the LF clock will already have switched
* and the interrupt will fire once interrupts are enabled
* again when the OS starts.
* When using a regular HF crystal, it may take a little
* time for the crystal to start up
*/
HWREG(PRCM_BASE + PRCM_O_OSCIMSC) |= PRCM_OSCIMSC_LFSRCDONEIM_M;
/* disallow standby since we cannot go into standby with
* an HF derived LF clock
*/
Power_setConstraint(PowerCC26XX_DISALLOW_STANDBY);
}
//CC_POWER_DRIVER_OPTIMIZATION - Do you use the VIMS RAM as GPRAM?
/* if VIMS RAM is configured as GPRAM: set retention constraint */
// if (!CCFGRead_DIS_GPRAM()) {
// Power_setConstraint(PowerCC26XX_RETAIN_VIMS_CACHE_IN_STANDBY);
// }
return (Power_SOK);
}
/*
* ======== Power_registerNotify ========
* Register a function to be called on a specific power event.
*
*/
int_fast16_t Power_registerNotify(Power_NotifyObj * pNotifyObj,
uint_fast16_t eventTypes, Power_NotifyFxn notifyFxn, uintptr_t clientArg)
{
int_fast16_t status = Power_SOK;
/* check for NULL pointers */
if ((pNotifyObj == NULL) || (notifyFxn == NULL)) {
status = Power_EINVALIDPOINTER;
}
else {
/* fill in notify object elements */
pNotifyObj->eventTypes = eventTypes;
pNotifyObj->notifyFxn = notifyFxn;
pNotifyObj->clientArg = clientArg;
/* place notify object on event notification queue */
List_put(&PowerCC26X2_module.notifyList, (List_Elem*)pNotifyObj);
}
return (status);
}
/*
* ======== Power_releaseConstraint ========
* Release a previously declared constraint.
*/
int_fast16_t Power_releaseConstraint(uint_fast16_t constraintId)
{
unsigned int key;
uint8_t count;
/* assert constraintId is valid */
DebugP_assert(constraintId < PowerCC26X2_NUMCONSTRAINTS);
key = HwiP_disable();
/* get the count of the constraint */
count = PowerCC26X2_module.constraintCounts[constraintId];
DebugP_assert(count != 0);
count--;
/* save the updated count */
PowerCC26X2_module.constraintCounts[constraintId] = count;
if (count == 0) {
PowerCC26X2_module.constraintMask &= ~(1 << constraintId);
}
HwiP_restore(key);
return (Power_SOK);
}
/*
* ======== Power_releaseDependency ========
* Release a previously declared dependency.
*/
int_fast16_t Power_releaseDependency(uint_fast16_t resourceId)
{
uint8_t parent;
uint8_t count;
uint32_t id;
unsigned int key;
/* assert resourceId is valid */
DebugP_assert(resourceId < PowerCC26X2_NUMRESOURCES);
/* disable interrupts */
key = HwiP_disable();
/* read and decrement the reference count */
count = PowerCC26X2_module.resourceCounts[resourceId];
DebugP_assert(count != 0);
count--;
/* save the reference count */
PowerCC26X2_module.resourceCounts[resourceId] = count;
/* if this was the last dependency being released.., */
if (count == 0) {
/* deactivate this resource ... */
id = resourceDB[resourceId].driverlibID;
/* is resource a peripheral?... */
if (resourceDB[resourceId].flags & PowerCC26XX_PERIPH) {
PRCMPeripheralRunDisable(id);
PRCMPeripheralSleepDisable(id);
PRCMPeripheralDeepSleepDisable(id);
PRCMLoadSet();
while (!PRCMLoadGet()) {
;
}
}
/* else, does resource require a special handler?... */
else if (resourceDB[resourceId].flags & PowerCC26XX_SPECIAL) {
/* call the special handler */
PowerCC26X2_module.resourceHandlers[id](PowerCC26XX_DISABLE);
}
/* else resource is a power domain */
else {
PRCMPowerDomainOff(id);
while (PRCMPowerDomainStatus(id) != PRCM_DOMAIN_POWER_OFF) {
;
}
}
/* propagate release up the dependency tree ... */
/* check for a first parent */
parent = resourceDB[resourceId].flags & PowerCC26XX_PARENTMASK;
/* if 1st parent, make recursive call to release that dependency */
if (parent < PowerCC26X2_NUMRESOURCES) {
Power_releaseDependency(parent);
}
}
/* re-enable interrupts */
HwiP_restore(key);
return (Power_SOK);
}
/*
* ======== Power_setConstraint ========
* Declare an operational constraint.
*/
int_fast16_t Power_setConstraint(uint_fast16_t constraintId)
{
unsigned int key;
/* assert constraint id is valid */
DebugP_assert(constraintId < PowerCC26X2_NUMCONSTRAINTS);
/* disable interrupts */
key = HwiP_disable();
/* set the specified constraint in the constraintMask */
PowerCC26X2_module.constraintMask |= 1 << constraintId;
/* increment the specified constraint count */
PowerCC26X2_module.constraintCounts[constraintId]++;
/* re-enable interrupts */
HwiP_restore(key);
return (Power_SOK);
}
/*
* ======== Power_setDependency ========
* Declare a dependency upon a resource.
*/
int_fast16_t Power_setDependency(uint_fast16_t resourceId)
{
uint8_t parent;
uint8_t count;
uint32_t id;
unsigned int key;
/* assert resourceId is valid */
DebugP_assert(resourceId < PowerCC26X2_NUMRESOURCES);
/* disable interrupts */
key = HwiP_disable();
/* read and increment reference count */
count = PowerCC26X2_module.resourceCounts[resourceId]++;
/* if resource was NOT activated previously ... */
if (count == 0) {
/* propagate set up the dependency tree ... */
/* check for a first parent */
parent = resourceDB[resourceId].flags & PowerCC26XX_PARENTMASK;
/* if first parent, make recursive call to set that dependency */
if (parent < PowerCC26X2_NUMRESOURCES) {
Power_setDependency(parent);
}
/* now activate this resource ... */
id = resourceDB[resourceId].driverlibID;
/* is resource a peripheral?... */
if (resourceDB[resourceId].flags & PowerCC26XX_PERIPH) {
PRCMPeripheralRunEnable(id);
PRCMPeripheralSleepEnable(id);
PRCMPeripheralDeepSleepEnable(id);
PRCMLoadSet();
while (!PRCMLoadGet()) {
;
}
}
/* else, does resource require a special handler?... */
else if (resourceDB[resourceId].flags & PowerCC26XX_SPECIAL) {
/* call the special handler */
PowerCC26X2_module.resourceHandlers[id](PowerCC26XX_ENABLE);
}
/* else resource is a power domain */
else {
PRCMPowerDomainOn(id);
while (PRCMPowerDomainStatus(id) != PRCM_DOMAIN_POWER_ON) {
;
}
}
}
/* re-enable interrupts */
HwiP_restore(key);
return (Power_SOK);
}
/*
* ======== Power_setPolicy ========
* Set the Power policy function
*/
void Power_setPolicy(Power_PolicyFxn policy)
{
PowerCC26X2_module.policyFxn = policy;
}
/*
* ======== Power_shutdown ========
*/
int_fast16_t Power_shutdown(uint_fast16_t shutdownState,
uint_fast32_t shutdownTime)
{
int_fast16_t status = Power_EFAIL;
unsigned int constraints;
unsigned int hwiKey;
/* disable interrupts */
hwiKey = HwiP_disable();
/* check if there is a constraint to prohibit shutdown */
constraints = Power_getConstraintMask();
if (constraints & (1 << PowerCC26XX_DISALLOW_SHUTDOWN)) {
status = Power_ECHANGE_NOT_ALLOWED;
}
/* OK to shutdown ... */
else if (PowerCC26X2_module.state == Power_ACTIVE) {
/* set new transition state to entering shutdown */
PowerCC26X2_module.state = Power_ENTERING_SHUTDOWN;
/* signal all clients registered for pre-shutdown notification */
status = notify(PowerCC26XX_ENTERING_SHUTDOWN);
/* check for any error */
if (status != Power_SOK) {
PowerCC26X2_module.state = Power_ACTIVE;
HwiP_restore(hwiKey);
return (status);
}
/* Ensure the JTAG domain is turned off
* otherwise MCU domain can't be turned off.
*/
HWREG(AON_PMCTL_BASE + AON_PMCTL_O_JTAGCFG) = 0;
SysCtrlAonSync();
/* now proceed with shutdown sequence ... */
SysCtrlShutdownWithAbort();
}
else {
status = Power_EBUSY;
}
/* NOTE: if shutdown succeeded, should never get here */
/* return failure status */
PowerCC26X2_module.state = Power_ACTIVE;
/* re-enable interrupts */
HwiP_restore(hwiKey);
/* if get here, failed to shutdown, return error code */
return (status);
}
/*
* ======== Power_sleep ========
*/
int_fast16_t Power_sleep(uint_fast16_t sleepState)
{
int_fast16_t status = Power_SOK;
int_fast16_t notifyStatus = Power_SOK;
int_fast16_t lateNotifyStatus = Power_SOK;
unsigned int xosc_hf_active = false;
uint_fast16_t postEventLate;
uint32_t poweredDomains = 0;
uint_fast16_t preEvent;
uint_fast16_t postEvent;
unsigned int constraints;
bool retainCache = false;
uint32_t modeVIMS;
unsigned int swiKey;
/* first validate the sleep code */
if (sleepState != PowerCC26XX_STANDBY) {
status = Power_EINVALIDINPUT;
}
else {
/* check to make sure Power is not busy with another transition */
if (PowerCC26X2_module.state == Power_ACTIVE) {
/* set transition state to entering sleep */
PowerCC26X2_module.state = Power_ENTERING_SLEEP;
}
else {
status = Power_EBUSY;
}
if (status == Power_SOK) {
/* setup sleep vars */
preEvent = PowerCC26XX_ENTERING_STANDBY;
postEvent = PowerCC26XX_AWAKE_STANDBY;
postEventLate = PowerCC26XX_AWAKE_STANDBY_LATE;
/* disable Task scheduling */
PowerCC26XX_schedulerDisable();
/* signal all clients registered for pre-sleep notification */
status = notify(preEvent);
/* check for any error */
if (status != Power_SOK) {
PowerCC26X2_module.state = Power_ACTIVE;
PowerCC26XX_schedulerRestore();
return (status);
}
/* now disable Swi scheduling */
swiKey = SwiP_disable();
/* 1. Query and save domain states before powering them off */
if (Power_getDependencyCount(PowerCC26XX_DOMAIN_RFCORE)) {
poweredDomains |= PRCM_DOMAIN_RFCORE;
}
if (Power_getDependencyCount(PowerCC26XX_DOMAIN_SERIAL)){
poweredDomains |= PRCM_DOMAIN_SERIAL;
}
if (Power_getDependencyCount(PowerCC26XX_DOMAIN_PERIPH)) {
poweredDomains |= PRCM_DOMAIN_PERIPH;
}
/* 2. If XOSC_HF is active or we are waiting to switch
* to it, force it off. Otherwise, the XOSC_HF may be
* automatically turned on by the hardware without
* a call to configureXOSCHF(PowerCC26XX_ENABLE)
* This is not necessarily a problem. However exactly
* what the cutoff point is where the hardware considers
* the XOSC_HF "on" without having switched to is not
* considered by this driver.
*/
// CC_POWER_DRIVER_OPTIMIZATION - What did you chose as HF Clock Source? (here HF Clock Source is OSC_RCOSC_HF)
if (/*OSCClockSourceGet(OSC_SRC_CLK_HF)*/ OSC_RCOSC_HF == OSC_XOSC_HF ||
PowerCC26X2_module.xoscPending == true) {
xosc_hf_active = true;
configureXOSCHF(PowerCC26XX_DISABLE);
}
/* query constraints to determine if cache should be retained */
constraints = Power_getConstraintMask();
if (constraints & (1 << PowerCC26XX_RETAIN_VIMS_CACHE_IN_STANDBY)) {
retainCache = true;
}
else {
retainCache = false;
// Get the current VIMS mode
do {
modeVIMS = VIMSModeGet(VIMS_BASE);
} while (modeVIMS == VIMS_MODE_CHANGING);
}
/* 3.
* - Freeze the IOs on the boundary between MCU and AON
* - Make sure AON writes take effect
* - Request power off of every PD in the MCU voltage domain
* - Ensure that no clocks are forced on in Crypto, DMA and I2S
* - Gate running deep sleep clocks for Crypto, DMA and I2S
* - Load the new clock settings
* - Configure the VIMS power domain mode to power up flash
* again after coming out of standby.
* - Request uLDO during standby
* - Use recharge comparator
* - Ensure all writes have taken effect
* - Ensure UDMA, Crypto and I2C clocks are turned off
* - Ensure all non-CPU power domains are turned off
* - Turn off cache retention if requested
* - Invoke deep sleep to go to standby
*/
SysCtrlStandby(retainCache,
VIMS_ON_CPU_ON_MODE,
SYSCTRL_PREFERRED_RECHARGE_MODE);
/* 4. If didn't retain VIMS in standby, re-enable retention now */
if (retainCache == false) {
/* 5.1 If previously in a cache mode, restore the mode now */
if (modeVIMS == VIMS_MODE_ENABLED) {
VIMSModeSet(VIMS_BASE, modeVIMS);
}
/* 5.2 Re-enable retention */
PRCMCacheRetentionEnable();
}
/* 6. Start re-powering power domains */
PRCMPowerDomainOn(poweredDomains);
/* 7. Restore deep sleep clocks of Crypto and DMA */
if (Power_getDependencyCount(PowerCC26XX_PERIPH_CRYPTO)) {
PRCMPeripheralDeepSleepEnable(
resourceDB[PowerCC26XX_PERIPH_CRYPTO].driverlibID);
}
if (Power_getDependencyCount(PowerCC26XX_PERIPH_UDMA)) {
PRCMPeripheralDeepSleepEnable(
resourceDB[PowerCC26XX_PERIPH_UDMA].driverlibID);
}
/* 8. Make sure clock settings take effect */
PRCMLoadSet();
/* 9. Release request for uLDO */
PRCMMcuUldoConfigure(false);
/* 10. Set transition state to EXITING_SLEEP */
PowerCC26X2_module.state = Power_EXITING_SLEEP;
/* 11. Wait until all power domains are back on */
while (PRCMPowerDomainStatus(poweredDomains) != PRCM_DOMAIN_POWER_ON);
/* 12. Wait for the RTC shadow values to be updated so that
* the early notification callbacks can read out valid RTC values.
* This can likely be removed as the 2MHz MF clock will have ticked by now.
*/
SysCtrlAonSync();
/*
* 13. Signal clients registered for early post-sleep notification;
* this should be used to initialize any timing critical or IO
* dependent hardware
*/
notifyStatus = notify(postEvent);
/* 14. Disable IO freeze and ensure RTC shadow value is updated */
AONIOCFreezeDisable();
SysCtrlAonSync();
/* 15. If XOSC_HF was forced off above, initiate switch back */
if (xosc_hf_active == true) {
configureXOSCHF(PowerCC26XX_ENABLE);
}
/* 16. Re-enable interrupts */
CPUcpsie();
/*
* 17. Signal all clients registered for late post-sleep
* notification
*/
lateNotifyStatus = notify(postEventLate);
/*
* 18. Now clear the transition state before re-enabling
* scheduler
*/
PowerCC26X2_module.state = Power_ACTIVE;
/* Re-enable Swi scheduling */
SwiP_restore(swiKey);
/* re-enable Task scheduling */
PowerCC26XX_schedulerRestore();
/* if there was a notification error, set return status */
if ((notifyStatus != Power_SOK) ||
(lateNotifyStatus != Power_SOK)) {
status = Power_EFAIL;
}
}
}
return (status);
}
/*
* ======== Power_unregisterNotify ========
* Unregister for a power notification.
*
*/
void Power_unregisterNotify(Power_NotifyObj * pNotifyObj)
{
unsigned int key;
/* remove notify object from its event queue */
key = HwiP_disable();
/* remove notify object from its event queue */
List_remove(&PowerCC26X2_module.notifyList, (List_Elem *)pNotifyObj);
HwiP_restore(key);
}
/* ****************** CC26XX specific APIs ******************** */
/*
* ======== PowerCC26XX_calibrate ========
* Plug this function into the PowerCC26X2_Config structure
* if calibration is needed.
*/
bool PowerCC26XX_calibrate(unsigned int arg)
{
bool retVal = false;
switch (arg) {
case PowerCC26X2_INITIATE_CALIBRATE:
retVal = PowerCC26X2_initiateCalibration();
break;
case PowerCC26X2_DO_CALIBRATE:
PowerCC26X2_calibrate();
break;
default:
while (1);
}
return (retVal);
}
/*
* ======== PowerCC26XX_doWFI ========
*/
void PowerCC26XX_doWFI(void)
{
__asm(" wfi");
}
/*
* ======== PowerCC26X2_getClockHandle ========
*/
ClockP_Handle PowerCC26XX_getClockHandle()
{
return ((ClockP_Handle)&PowerCC26X2_module.clockObj);
}
/*
* ======== PowerCC26XX_noCalibrate ========
* Plug this function into the PowerCC26X2 config structure if calibration
* is not needed.
*/
bool PowerCC26XX_noCalibrate(unsigned int arg)
{
return (0);
}
/*
* ======== PowerCC26XX_getXoscStartupTime ========
* Get the estimated crystal oscillator startup time
*/
uint32_t PowerCC26XX_getXoscStartupTime(uint32_t timeUntilWakeupInMs)
{
return (OSCHF_GetStartupTime(timeUntilWakeupInMs));
}
/*
* ======== PowerCC26X2_injectCalibration ========
* Explicitly trigger RCOSC calibration
*/
bool PowerCC26XX_injectCalibration(void)
{
if ((*(PowerCC26X2_config.calibrateFxn))(PowerCC26X2_INITIATE_CALIBRATE)) {
/* here if AUX SMPH was available, start calibration now ... */
(*(PowerCC26X2_config.calibrateFxn))(PowerCC26X2_DO_CALIBRATE);
return (true);
}
return (false);
}
/*
* ======== PowerCC26XX_isStableXOSC_HF ========
* Check if XOSC_HF has stabilized.
*/
bool PowerCC26XX_isStableXOSC_HF(void)
{
bool ready = true;
unsigned int key;
key = HwiP_disable();
/* only query if HF source is ready if there is a pending change */
if (PowerCC26X2_module.xoscPending) {
ready = OSCHfSourceReady();
}
HwiP_restore(key);
return (ready);
}
/*
* ======== PowerCC26XX_switchXOSC_HF ========
* Switch to enable XOSC_HF.
* May only be called when using the PowerCC26XX_SWITCH_XOSC_HF_MANUALLY
* constraint.
* May only be called after ensuring the XOSC_HF is stable by calling
* PowerCC26XX_isStableXOSC_HF().
*/
void PowerCC26XX_switchXOSC_HF(void)
{
bool readyToCal;
unsigned int key;
key = HwiP_disable();
/* Since PowerCC26X2_isStableXOSC_HF() should have been called before this
* function, we can just switch without handling the case when the XOSC_HF
* is not ready or PowerCC26X2_module.xoscPending is not true.
*/
OSCHF_AttemptToSwitchToXosc();
/* Since configureXOSCHF() was called prior to this function to turn
* on the XOSC_HF, PowerCC26X2_module.xoscPending will be true and
* we can safely set it to false.
*/
PowerCC26X2_module.xoscPending = false;
/* Allow going into IDLE again since we sucessfully switched
* to XOSC_HF
*/
Power_releaseConstraint(PowerCC26XX_DISALLOW_IDLE);
HwiP_restore(key);
/* initiate RCOSC calibration */
readyToCal = (*(PowerCC26X2_config.calibrateFxn))(PowerCC26X2_INITIATE_CALIBRATE);
/* now notify clients that were waiting for a switch notification */
notify(PowerCC26XX_XOSC_HF_SWITCHED);
/* if ready to start first cal measurment, do it now */
if (readyToCal == true) {
(*(PowerCC26X2_config.calibrateFxn))(PowerCC26X2_DO_CALIBRATE);
}
}
/* * * * * * * * * * * internal and support functions * * * * * * * * * * */
/*
* ======== oscillatorISR ========
*/
static void oscillatorISR(uintptr_t arg)
{
uint32_t rawStatus = HWREG(PRCM_BASE + PRCM_O_OSCRIS);
uint32_t intStatusMask = HWREG(PRCM_BASE + PRCM_O_OSCIMSC);
/* Turn off mask for all flags we will handle */
HWREG(PRCM_BASE + PRCM_O_OSCIMSC) = intStatusMask & ~rawStatus;
/* XOSC_LF or RCOSC_LF qualified */
if (rawStatus & PRCM_OSCRIS_LFSRCDONERIS_M & intStatusMask) {
disableLFClockQualifiers();
}
/* XOSC_HF ready to switch to */
if (rawStatus & PRCM_OSCIMSC_HFSRCPENDIM_M & intStatusMask) {
switchXOSCHF();
}
/* Clear flags we will handle. Does not really work as expected as
* the flags seem to level-detect and not edge-detect. Until the
* underlying trigger is taken care of, the flag will not deassert
* even when cleared.
* We're clearing at the end in order to prevent the flag from
* immediately asserting again if the underlying trigger was
* not handled yet.
* SCLK_LF switched can never be cleared after triggering
* only masked out. XOSC_HF ready to switch can be cleared
* after switching to XOSC_HF.
*/
HWREG(PRCM_BASE + PRCM_O_OSCICR) = intStatusMask & rawStatus;
}
/*
* ======== emptyClockFunc ========
* Clock function used by power policy to schedule early wakeups.
*/
static void emptyClockFunc(uintptr_t arg)
{
}
/*
* ======== disableLFClockQualifiers ========
* Clock function used for delayed disable of LF clock qualifiers.
*/
static void disableLFClockQualifiers(void)
{
uint32_t sourceLF;
/* query LF clock source */
// CC_POWER_DRIVER_OPTIMIZATION - What did you chose as LF Clock Source? (here LF Clock Source is OSC_XOSC_LF)
// sourceLF = OSCClockSourceGet(OSC_SRC_CLK_LF);
sourceLF = OSC_XOSC_LF;
/* is LF source either RCOSC_LF or XOSC_LF yet? */
if ((sourceLF == OSC_RCOSC_LF) || (sourceLF == OSC_XOSC_LF)) {
/* yes, disable the LF clock qualifiers */
DDI16BitfieldWrite(
AUX_DDI0_OSC_BASE,
DDI_0_OSC_O_CTL0,
DDI_0_OSC_CTL0_BYPASS_XOSC_LF_CLK_QUAL_M|
DDI_0_OSC_CTL0_BYPASS_RCOSC_LF_CLK_QUAL_M,
DDI_0_OSC_CTL0_BYPASS_RCOSC_LF_CLK_QUAL_S,
0x3
);
/* enable clock loss detection */
OSCClockLossEventEnable();
/* now finish by releasing the standby disallow constraint */
Power_releaseConstraint(PowerCC26XX_DISALLOW_STANDBY);
}
else if(sourceLF == OSC_XOSC_HF) {
/* yes, disable the LF clock qualifiers */
DDI16BitfieldWrite(
AUX_DDI0_OSC_BASE,
DDI_0_OSC_O_CTL0,
DDI_0_OSC_CTL0_BYPASS_XOSC_LF_CLK_QUAL_M|
DDI_0_OSC_CTL0_BYPASS_RCOSC_LF_CLK_QUAL_M,
DDI_0_OSC_CTL0_BYPASS_RCOSC_LF_CLK_QUAL_S,
0x3
);
/* enable clock loss detection */
OSCClockLossEventEnable();
/* do not allow standby since the LF clock is HF derived */
}
}
/*
* ======== nopResourceFunc ========
* special resource handler
*/
static unsigned int nopResourceHandler(unsigned int action)
{
return (0);
}
/*
* ======== notify ========
* Send notifications to registered clients.
* Note: Task scheduling is disabled when this function is called.
*/
static int_fast16_t notify(uint_fast16_t eventType)
{
int_fast16_t notifyStatus;
Power_NotifyFxn notifyFxn;
uintptr_t clientArg;
List_Elem *elem;
/* if queue is empty, return immediately */
if (!List_empty(&PowerCC26X2_module.notifyList)) {
/* point to first client notify object */
elem = List_head(&PowerCC26X2_module.notifyList);
/* walk the queue and notify each registered client of the event */
do {
if (((Power_NotifyObj *)elem)->eventTypes & eventType) {
/* pull params from notify object */
notifyFxn = ((Power_NotifyObj *)elem)->notifyFxn;
clientArg = ((Power_NotifyObj *)elem)->clientArg;
/* call the client's notification function */
notifyStatus = (int_fast16_t)(*(Power_NotifyFxn)notifyFxn)(
eventType, 0, clientArg);
/* if client declared error stop all further notifications */
if (notifyStatus != Power_NOTIFYDONE) {
return (Power_EFAIL);
}
}
/* get next element in the notification queue */
elem = List_next(elem);
} while (elem != NULL);
}
return (Power_SOK);
}
/*
* ======== configureRFCoreClocks ========
* Special dependency function for controlling RF core clocks.
* This function does nothing, but is kept for legacy reasons.
* All functionality has been integrated into the RF driver.
*/
static unsigned int configureRFCoreClocks(unsigned int action)
{
return (0);
}
/*
* ======== switchXOSCHF ========
* Switching to XOSC_HF when it has stabilized.
*/
static void switchXOSCHF(void)
{
bool readyToCal;
unsigned int key;
key = HwiP_disable();
/* Switch to the XOSC_HF. Since this function is only called
* after we get an interrupt signifying it is ready to switch,
* it should always succeed.
* If it does not succeed, try again. It is fine if we spin,
* there is no sensible recovery mechanism from such an error.
*/
while (!OSCHF_AttemptToSwitchToXosc());
/* The only time we should get here is when PowerCC26X2_module.xoscPending == true
* holds.
* Allow going into IDLE again since we sucessfully switched
* to XOSC_HF
*/
Power_releaseConstraint(PowerCC26XX_DISALLOW_IDLE);
PowerCC26X2_module.xoscPending = false;
HwiP_restore(key);
/* initiate RCOSC calibration */
readyToCal = (*(PowerCC26X2_config.calibrateFxn))(PowerCC26X2_INITIATE_CALIBRATE);
/* now notify clients that were waiting for a switch notification */
notify(PowerCC26XX_XOSC_HF_SWITCHED);
/* if ready to start first cal measurment, do it now */
if (readyToCal == true) {
(*(PowerCC26X2_config.calibrateFxn))(PowerCC26X2_DO_CALIBRATE);
}
}
/*
* ======== configureXOSCHF ========
*/
static unsigned int configureXOSCHF(unsigned int action)
{
/* By checking action == PowerCC26XX_ENABLE and PowerCC26X2_module.xoscPending
* carefully, the function should be idempotent. Calling it with the same
* action more than once will not have any effect until the hardware triggers
* a software state change.
*/
// CC_POWER_DRIVER_OPTIMIZATION - What did you chose as HF Clock Source? (here HF Clock Source is OSC_RCOSC_HF)
if (action == PowerCC26XX_ENABLE &&
/*OSCClockSourceGet(OSC_SRC_CLK_HF)*/ OSC_RCOSC_HF != OSC_XOSC_HF &&
PowerCC26X2_module.xoscPending == false) {
/* Check if TCXO is selected in CCFG and in addition configured to be enabled
* by the function pointed to by PowerCC26X2_config.enableTCXOFxn.
*/
// CC_POWER_DRIVER_OPTIMIZATION - Have you enable a TCXO function? / Are you using the TCXO?
// if ((CCFGRead_XOSC_FREQ() == CCFGREAD_XOSC_FREQ_TCXO) &&
// (PowerCC26X2_config.enableTCXOFxn != NULL)) {
//
// /* Enable power on TCXO */
// (*(PowerCC26X2_config.enableTCXOFxn))(true);
//
// /* Configure TCXO */
// HWREG(AUX_DDI0_OSC_BASE + DDI_O_CLR + DDI_0_OSC_O_CTL0) = DDI_0_OSC_CTL0_XTAL_IS_24M;
// HWREG(AUX_DDI0_OSC_BASE + DDI_O_SET + DDI_0_OSC_O_XOSCHFCTL) = DDI_0_OSC_XOSCHFCTL_BYPASS;
// if (CCFGRead_TCXO_TYPE() == 0x1)
// {
// /* Selected TCXO type is clipped-sine. Enabled internal common-mode bias. */
// HWREG( AUX_DDI0_OSC_BASE + DDI_O_SET + DDI_0_OSC_O_XOSCHFCTL ) = DDI_0_OSC_XOSCHFCTL_TCXO_MODE_XOSC_HF_EN;
// }
//
// /* Start clock to wait for TCXO startup time before clock switch
// * can be attempted.
// */
// ClockP_start(ClockP_handle(&PowerCC26X2_module.tcxoEnableClock));
// }
OSCHF_TurnOnXosc();
PowerCC26X2_module.xoscPending = true;
/* Unless it is disallowed, unmask the XOSC_HF ready to switch flag */
// CC_POWER_DRIVER_OPTIMIZATION - Have you enable a TCXO function? / Are you using the TCXO?
// if (!((CCFGRead_XOSC_FREQ() == CCFGREAD_XOSC_FREQ_TCXO) &&
// (PowerCC26X2_config.enableTCXOFxn != NULL)))
// {
if (!(Power_getConstraintMask() & (1 << PowerCC26XX_SWITCH_XOSC_HF_MANUALLY))) {
/* Clearing the flag in the ISR does not always work. Clear it again just in case */
HWREG(PRCM_BASE + PRCM_O_OSCICR) = PRCM_OSCICR_HFSRCPENDC_M;
/* Turn on oscillator interrupt for SCLK_HF switching */
HWREG(PRCM_BASE + PRCM_O_OSCIMSC) |= PRCM_OSCIMSC_HFSRCPENDIM_M;
}
// }
/* If the device goes into IDLE in between turning on XOSC_HF and
* and switching SCLK_HF to XOSC_HF, the INT_OSC_COMB HFSRCPEND
* trigger will be suppressed.
* The DISALLOW_IDLE constraint should only ever be set whenever
* we transition from xoscPending == false to true.
*/
Power_setConstraint(PowerCC26XX_DISALLOW_IDLE);
}
/* when release XOSC_HF, auto switch to RCOSC_HF */
else if (action == PowerCC26XX_DISABLE) {
OSCHF_SwitchToRcOscTurnOffXosc();
/* Handle TCXO if selected in CCFG */
// CC_POWER_DRIVER_OPTIMIZATION - Have you enable a TCXO function? / Are you using the TCXO?
// if (CCFGRead_XOSC_FREQ() == CCFGREAD_XOSC_FREQ_TCXO) {
//
// /* Turn off bias if clipped sine TCXO type */
// if (CCFGRead_TCXO_TYPE() == 1) {
// HWREG(AUX_DDI0_OSC_BASE + DDI_O_CLR + DDI_0_OSC_O_XOSCHFCTL) =
// DDI_0_OSC_XOSCHFCTL_TCXO_MODE_XOSC_HF_EN;
// }
//
// /* Check if function for enabling/disabling TCXO is supported */
// if (PowerCC26X2_config.enableTCXOFxn != NULL) {
//
// /* Disable TCXO by turning off power */
// (*(PowerCC26X2_config.enableTCXOFxn))(false);
// }
// }
/* If we have not actually switched to XOSC_HF yet, we need to
* undo what we did above when turning on XOSC_HF. Otherwise,
* we may not balance the constraints correctly or get
* unexpected interrupts.
*/
if (PowerCC26X2_module.xoscPending) {
/* Remove HFSRCPEND from the OSC_COMB interrupt mask */
uint32_t oscMask = HWREG(PRCM_BASE + PRCM_O_OSCIMSC);
HWREG(PRCM_BASE + PRCM_O_OSCIMSC) = oscMask & ~ PRCM_OSCIMSC_HFSRCPENDIM_M;
/* Clear any residual trigger for HFSRCPEND */
HWREG(PRCM_BASE + PRCM_O_OSCICR) = PRCM_OSCICR_HFSRCPENDC;
Power_releaseConstraint(PowerCC26XX_DISALLOW_IDLE);
PowerCC26X2_module.xoscPending = false;
}
}
return (0);
}
/*
* ======== switchToTCXO ========
* Switching to TCXO after TCXO startup time has expired.
*/
// CC_POWER_DRIVER_OPTIMIZATION - Have you enable a TCXO function? / Are you using the TCXO?
//static void switchToTCXO(void)
//{
// /* Enable clock qualification on 48MHz signal from TCXO */
// HWREG( AUX_DDI0_OSC_BASE + DDI_O_SET + DDI_0_OSC_O_XOSCHFCTL ) = DDI_0_OSC_XOSCHFCTL_TCXO_MODE;
//
// /* Switch to TCXO */
// switchXOSCHF();
//}
Once again, these guidelines can be adapted to any device and any driver!