Tool/software: WEBENCH® Design Tools
Hi,
I am using cc2541. I am working on the pairing process. I am using the following commands and successfully able to pair device by entering
123456 code.
// Setup the GAP Bond Manager
{
uint32 passkey = 123456; // passkey "000000"
uint8 pairMode = GAPBOND_PAIRING_MODE_WAIT_FOR_REQ;
uint8 mitm = TRUE;
uint8 ioCap = GAPBOND_IO_CAP_DISPLAY_ONLY;
uint8 bonding = TRUE;
GAPBondMgr_SetParameter( GAPBOND_DEFAULT_PASSCODE, sizeof ( uint32 ), &passkey );
GAPBondMgr_SetParameter( GAPBOND_PAIRING_MODE, sizeof ( uint8 ), &pairMode );
GAPBondMgr_SetParameter( GAPBOND_MITM_PROTECTION, sizeof ( uint8 ), &mitm );
GAPBondMgr_SetParameter( GAPBOND_IO_CAPABILITIES, sizeof ( uint8 ), &ioCap );
GAPBondMgr_SetParameter( GAPBOND_BONDING_ENABLED, sizeof ( uint8 ), &bonding );
}
NOW my question is how can I pair directly without entering that code?
As some Bluetooth devices initialize pairing request and we just accept request and device become paired.
How can I do that in cc2541?
Thanks!