Other Parts Discussed in Thread: CC2564
Tool/software: TI C/C++ Compiler
HI, I use the TI HIDdemo of CC2564B of STM32,Now I set the cc2564 module to devie,The cc2564module has been connected to the PC。When the PC is connected to the HID of cc2564 module, I need to obtain the type of device, so that I can judge that the device is a PC device, and it is forbidden to use the mobile device to establish a connection with C2564 module,
My question is which subroutine can I use to get the type of connected device?