Part Number: CC2640R2F
Other Parts Discussed in Thread: TPS62740, UNIFLASH
Hello,
I'm using the CC2640r2 (via the SaBLEx-R2 module) for a new instrument. I've configured the module as shown in the schematic. When the device is connected via the debug connector to the XDS110 debugger on the LAUNCHXL Launch Pad, I can successfully download and run the program. When I power the board via external power (3AAA batteries), the system no longer advertises. I use a TPS62740 regulator to source current to the balance of the system and I have the enable pin pulled high via IO pin on CC2640r2. Can anyone see where I may have made a mistake?
Thanks for the help.
PatrickController - Rev2.pdf