Part Number: LAUNCHXL-CC26X2R1
Hi Team,
Hardware: CC26X2 launchpad
Software: simplelink_cc13x2_26x2_sdk_4_10_00_78
A customer used 5 launchpad to test multiple AOA connection, and set connect_interval_mSec = 500 in python. The result is as following figures:


The passive role could connect and measure angles, but it got disconnected from time to time. He tried multiple times and this situation continued.
1.If only set up master and passive, the connection wouldn't lose.
2.Only the passive role got disconnected, no other roles. And it only happened when master and passive were both doing measurement.
3.This problem occurred in SDK 4.1, he tested on SDK3.4 and everything was fine.
Does the SDK updating cause this prblem?
BR,
Viki