IN my code, PIN_setInterrupt() is used to disable the interrupt for a specific pin.
However, I need to use PIN_setInterrupt() multiple times to enable the interrupt for a specific PIN even if sometimes the itnerrupt for this pin is already enabled. Calling PIN_setInterrupt() multiple times to enable the interrupt for the same pin for which the interrupt is also enabled causes any issue?
I am using SDK v3.20.