Hi
I am using the cc13x2 cc26x2 sdk rev 4.10.0.78
c26x2r1 launchxl with launchpad cc2640r2 one board with rtls_master firmware and one board with rtls_slave firmware
to the board with the rtls_master I need to connect my switch and antennas set con, the switch is connected to different IO pins
where can I define the new pins in order to perform AOA
thanks
Zahiz