Part Number: LP-CC2652RB
Other Parts Discussed in Thread: CC2652RB
Tool/software: Code Composer Studio
Hello,
I have an application to write incoming uart data to an sd card. For this application i have tried to merge uartecho & fatsd but unable to do it.
Can someone suggest me how to proceed ahead?
I am attaching the developed code in txt file.
I am not getting any message in the sd card.
#include <file.h>
#include <stdbool.h>
#include <stdint.h>
#include <stddef.h>
#include <stdio.h>
#include <stdlib.h>
#include <string.h>
#include <time.h>
#include <third_party/fatfs/ffcio.h>
/* Driver Header files */
#include <ti/display/Display.h>
#include <ti/drivers/GPIO.h>
#include <ti/drivers/UART.h>
#include <ti/drivers/SDFatFS.h>
/* Driver configuration */
#include "ti_drivers_config.h"
/* Buffer size used for the file copy process */
#ifndef CPY_BUFF_SIZE
#define CPY_BUFF_SIZE 2048
#endif
/* String conversion macro */
#define STR_(n) #n
#define STR(n) STR_(n)
/* Drive number used for FatFs */
#define DRIVE_NUM 0
const char inputfile[] = "fat:"STR(DRIVE_NUM)":input.txt";
char textarray[100];
static Display_Handle display;
/* File name prefix for this filesystem for use with TI C RTS */
char fatfsPrefix[] = "fat";
unsigned char cpy_buff[CPY_BUFF_SIZE + 1];
void *mainThread(void *arg0)
{
char input;
unsigned int i=0;
UART_Handle uart;
UART_Params uartParams;
SDFatFS_Handle sdfatfsHandle;
/* Variables for the CIO functions */
FILE *src;
unsigned int filesize;
/* Call driver init functions */
GPIO_init();
UART_init();
Display_init();
SDFatFS_init();
/* Configure the LED pin */
GPIO_setConfig(CONFIG_GPIO_LED_0, GPIO_CFG_OUT_STD | GPIO_CFG_OUT_LOW);
/* add_device() should be called once and is used for all media types */
add_device(fatfsPrefix, _MSA, ffcio_open, ffcio_close, ffcio_read,
ffcio_write, ffcio_lseek, ffcio_unlink, ffcio_rename);
/* Turn on user LED */
GPIO_write(CONFIG_GPIO_LED_0, CONFIG_GPIO_LED_ON);
/* Create a UART with data processing off. */
UART_Params_init(&uartParams);
uartParams.writeDataMode = UART_DATA_BINARY;
uartParams.readDataMode = UART_DATA_BINARY;
uartParams.readReturnMode = UART_RETURN_FULL;
uartParams.baudRate = 115200;
uart = UART_open(CONFIG_UART_0, &uartParams);
if (uart == NULL) {
/* UART_open() failed */
while (1);
}
/* Loop forever echoing */
while (1)
{
/* Mount and register the SD Card */
sdfatfsHandle = SDFatFS_open(CONFIG_SDFatFS_0, DRIVE_NUM);
if (sdfatfsHandle == NULL) {
Display_printf(display, 0, 0, "Error starting the SD card\n");
while (1);
}
else {
Display_printf(display, 0, 0, "Drive %u is mounted\n", DRIVE_NUM);
}
for (i=0; i < strlen (textarray); i++ )
{
char c = UART_read(uart, &input, 1);
UART_write(uart, &input, 1);
textarray [i] = c;
}
/* Try to open the source file */
src = fopen(inputfile, "r");
if (!src) {
Display_printf(display, 0, 0, "Creating a new file \"%s\"...", inputfile);
/* Open file for both reading and writing */
src = fopen(inputfile, "w+");
if (!src) {
Display_printf(display, 0, 0, "Error: \"%s\" could not be created.\nPlease check the "
"Board.html if additional jumpers are necessary.\n",
inputfile);
Display_printf(display, 0, 0, "Aborting...\n");
while (1);
}
fwrite (textarray,1,strlen(textarray),src);
fflush(src);
/* Reset the internal file pointer */
rewind(src);
Display_printf(display, 0, 0, "done\n");
}
else {
Display_printf(display, 0, 0, "Using existing copy of \"%s\"\n",
inputfile);
}
}
}
/*
* ======== fatfs_getFatTime ========
*/
int32_t fatfs_getFatTime(void)
{
/*
* FatFs uses this API to get the current time in FatTime format. User's
* must implement this function based on their system's timekeeping
* mechanism. See FatFs documentation for details on FatTime format.
*/
/* Jan 1 2017 00:00:00 */
return (0x4A210000);
}