Part Number: BOOSTXL-AOA
Tool/software: Code Composer Studio
We are trying to run angle of arrival using the following hardware/software:
AoA BOOSTXL - AoA
CC2640R2 (following this specs http://dev.ti.com/tirex/explore/node?node=AHckEvhg0Y3xs5rlangU2w__FUz-xrs__LATEST)
simplelink_cc2640r2_sdk_3_20_00_21
rtls_agent_cli.exe
The results are somewhat strange:
- We can not run AoA feature
- RSSI values are very small even though the distance between transmitter and receiver are 30cm
- We loose the connection when the distance between transmitter and receiver is above around 1m
(see screen below)
We managed to run older version of AoA measurement using the same hardware, that is:
AoA BOOSTXL - AoA
CC2640R2 (following this specs http://dev.ti.com/tirex/explore/node?node=AHckEvhg0Y3xs5rlangU2w__FUz-xrs__LATEST)
but with the following software version:
simplelink_cc2640r2_sdk_2_30_00_28
We got AoA data, but RSSI signal was also very low.
I have the following questions:
1) Do we use right hardware + software combination?
2) Are these RSSI values correct (we do not get results for distances >1m)?
3) Why is it impossible to measure AoA using cc2640r2_sdk_3_20_00_21 software? Is it necessary to add Passive device? What hardware should we use for this purpose?