Hello,
I am using CCS Version 10.1.0, XDCTools version 3.61.01.25, Simplelink SDK Version 4.20.00.35, and am compiling my project with TI v20.2.1.LTS. My OS is 64-bit Windows 10. My target device is CC2652R1F. I am programming it via the JTAG interface on the Launchpad.
In developing my Bluetooth application, I have been reviewing the Linker Command File for the Simple Peripheral example project. I noticed a couple input/output sections that I have not been able to find any documentation on. These include ".constdata", ".rodata", and ".emb_text". I have already reviewed the ARM Assembly Language Tools User's Guide, ARM Optimizing C/C++ Compiler User's Guide, and the ARM Compiler User's Guide without any luck. Are these sections created in one of the BLE stack libraries or are they entirely unnecessary? I am worried that not allocating them in my linker command file might cause arcane errors to be thrown by the stack.
Thank you for the assistance.