This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

CC2652R: CCS/CC2652R: CCS/CC2652R: Can we change CTE frame interval less than 100ms (ex: 10ms or 20ms)

Intellectual 1715 points

Replies: 6

Views: 68

Part Number: CC2652R

Hi Team,

As title.

Gary Lin, 林忠衡

Connectivity, EPD

Company Mobile : +886 90979 2810

Office Telephone : +886 22175 2810

Personal Mobile : +886 952276831

Address:

Texas Instruments Taiwan, Hung Tai Center Building
13F, 168, Tun-Hua North Road, 10548, Taipei, Taiwan

  • Gary,

    Would you please indicate what SDK you're working with?

    I've assigned someone to help you.

    -Luis

  • Hi,

    I answered this question in one of the threads linked.

    To complete the answer, you can use the function RTLSCtrl_updateConnInterval() (in rtls_ctrl.c) to update the connection interval.

    Regards,

    - Clément

  • In reply to Clément:

    Hi Clément,

    What is the unit of this API?  100ms?

    RTLSCtrl_updateConnInterval()

  • In reply to Valery Wu:

    Hi Valery,

    The connection interval is in units of 1.25ms

    Best regards,

    - Clément

  • In reply to Clément:

    thx Clément

    I have follow below discussion to changed interval on python script. it is useful, but interval unit should be 1ms?

    e2e.ti.com/.../859434

  • In reply to Valery Wu:

    Hi,

    I think you are right for the python script but not in the code.

    I agree this is not properly documented and I will open an internal ticket to improve this.

    Regards,

    - Clément

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.