This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] Bluetooth Low Energy Development Guidelines

Other Parts Discussed in Thread: SYSCONFIG

This guide is intended to provide a reference for all stages of development using TI Bluetooth® Low Energy connectivity products.

Step 0: Learn the technology

Step 1: Pick your device

Step 2: Download necessary software

Step 3: Begin software development

Step 4: Deep-dive into documentation

Step 5: Design your hardware

Step 6: Certification and production

Also see the ‘Common Development Questions’ section at the end.

 

Not sure what connectivity technology to use? Check out the Wireless Connectivity Technology Selection Guide!

 

Step 0: Learn the technology

Step 1: Pick your device

* indicates newest device/family

Step 2: Download necessary software

Step 3: Begin software development

  • Out of Box Experience (CC2340Rx | CC13X2/26X2 | CC2640R2): Once you have selected your LaunchPad, learn about its features and run your first application!
  • Quick Start Guide (CC2340Rx | CC13X2/26X2 | CC2640R2): This guide provides a roadmap to the Bluetooth  Low Energy /Bluetooth  Low Energy 5 stack development environment. Get started using TI Resource Explorer, learn how to import a project into CCS or IAR, or develop a new application.
  • SimpleLink Academy (CC2340Rx | CC13X2/26X2 | CC2640R2):  Check out the SimpleLink Academy training platform for step-by-step instructions to learn about Bluetooth features and how to customize your application.

Lab

Description

Bluetooth Low Energy Fundamentals

(CC2340Rx | CC13X2/26X2 | CC2640R2)

Get started with Bluetooth by flashing a basic BLE example.

Bluetooth Low Energy 5 PHY

(CC2340Rx)

Configure and switch physical layers (PHY) in Bluetooth Low Energy

Bluetooth Low Energy Enhanced Over the Air Download Fundamentals

(CC2340Rx)

Learn how to wirelessly update firmware via the Over The Air Download (OAD) feature of the TI BLE5-Stack

Bluetooth Low Energy Security Fundamentals

(CC2340Rx)

Learn the Basics of the Security Features built into the TI BLE5-Stack

DMM Fundamentals

(CC2340Rx | CC13X2/26X2)

Dynamic Multi-protocol Manager (DMM) allows multiple wireless stacks to coexist and operate concurrently on a single radio

Sensor Controller Fundamentals

(CC13X2/26X2 | CC2640R2)

How to use the Sensor Controller Studio and GUI tool

RTOS Concepts

(CC13X2/26X2 | CC2640R2)

A general overview of concepts used in Real-Time Operating Systems such as task/threads, scheduling, semaphore. Start here to learn about TI-RTOS and POSIX.

SysConfig Tool Basics

(CC13X2/26X2 | CC2640R2)

SysConfig is tool to help you configure your SimpleLink applications, generating source files for TI Drivers and software libraries

 

Step 4: Deep-dive into documentation

Step 5: Design your hardware

Step 6: Certification and production

 

Common Development Questions

  • How do I get started?

Start with the Out of Box Experience! This demo helps you learn about your LaunchPad and run your first application. After that, start to learn about the different features and software libraries we provide on SimpleLink Academy.                                                                                                                                                 

  • How do I add my technology to a new application?

It is recommended that users start with one of the various development examples provided in the SDK.

  • How do I learn about the peripheral drivers? Where do I find examples for PWM, I2C, SPI, UART, or GPIOs?

The TI Drivers Runtime APIs provide basic usage summaries and examples for each peripheral, and additional TI Drivers examples are provided for each device inside the examples/<rtos>/<LaunchPad>/drivers folder of your SDK.

  • How do I flash code to my LaunchPad?

Use the CCSTUDIO IDE to build, load, and debug code. To program a binary image on a 2.4 or Sub1-GHZ device, refer to either FLASH-PROGRAMMER or UNIFLASH.

  • Where do I learn about security features?

Find out more about the SimpleLink security features available on each stack with these White Papers.

  • How do I get a schematic and layout review?

Design reviews can be requested for Sub-1 GHz and 2.4 GHz hardware

  • Where do I go for help? Where can I find more FAQs?

The E2E Wireless Connectivity forum is the go-to source for help throughout every step of the design process.

E2E is a public forum with questions and answers posted by TI engineers  and knowledgeable community members to help users quickly solve their design issues. Search a few keywords to see resolved questions, or you can ask a new question!