Hi,
Does CC2564C support BCM58201 from Broadcom?
If not, is there any method to support it as non-OS based?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Does CC2564C support BCM58201 from Broadcom?
If not, is there any method to support it as non-OS based?
Thanks.
Hi,
What architecture is the BCM58201? It doesn't appear that the datasheet for that device is publicly available.
In general, the CC2564C is a BT5.1 compliant controller, and can support any device that is able to interface with it over UART to send it the HCI commands needed.
If you want to use the TI-provided free Bluetooth stack, Bluetopia, then only certain architectures are supported, namely the ARM Cortex M4 and A7 architectures. Please take a look at the FAQ here for more information:
Let me know if you need more clarification or have further questions on getting the CC2564C working with that Broadcom MPU.
Regards,
Michael