Other Parts Discussed in Thread: CC2640, CC2650, CC2540, LAUNCHXL-CC2640R2, CC2640R2F, LAUNCHXL-CC26X2R1
HCI Tester
HCI Tester is a Windows PC scripting tool which will send/receive serial HCI packets to CC254X or CC2640/CC2650. This can be use to control a supported BLE device which is programmed with HostTestRelease hex file.
HCI Tester will work with the following configurations
- PC to CC2540 USB Dongle
- PC to CC254X EM on SmartRF board (over USB to Serial Cable)
- PC to CC254X with UART pins connected
- PC to CC2640 with UART pins connected (e.g., CC2650DK with COM port exposed via USB JTAG connection)
- PC to CC2640R2F with UART pins connected (e.g., LAUNCHXL-CC2640R2 with COM port exposed via XDS110 connection)
- PC to CC26x2 with UART pins connected (e.g., LAUNCHXL-CC26X2R1 with COM port exposed via XDS110 connection)
Overview
Program USB Dongle, KeyFob or Launchpad
See QuickStart guide on how to program USB Dongle and KeyFob. QuickStartGuide
A prebuilt HostTestrelease hex can be found in the accessories folder.
<install>/BLE-CC254x-x.x.x/Accessories/HexFiles/CC2540_USBdongle_HostTestRelease_All.hex
A prebuilt SimpleBlePeripheral hex can be found in the accessories folder.
<install>/BLE-CC254x-x.x.x/Accessories/HexFiles/CC2540_SimpleBlePeripheral.hex
For CC2640R2 and CC26x2 devices, you can use the host_test example. A prebuilt hex is available in your SDK.
Download, Install and Configure HCI Tester
There is no official support for this tool, but you can download it from the WILINK-BT_WIFI-WIRELESS_TOOLS page.
One installed, you will need configure HCITester to point to the latest .XML library file. This file contains all of the supported HCI commands. Click on the middle icon in the Command Library pane to change HCI libraries.
The following are the HCITester library files for the respective BLE wireless MUCs and supported protocol stack versions:
CC254x:
20170119182836!HCITesterXML.zip
CC26xx:
20171128003351!HCITesterXML.zip
7167.HCITesterXML.zip
CC2640R2 and CC26x2:
Tester_HCILib_blestack_3_x.xml
Tester_HCILib_ble5stack_2_02_00_00.xml
Running HCI Tester
Once configured, goto menu and select com port.
Note for CC2640: Use "Flow Control" set to 'None' in the Serial Port setup menu.

Download this script file which contains the central commands to discover, connect and pair with SimpleBlePeripheral running on the keyFob.
Central_commands_sbp.zip
Advertise and Connect
If using keyFob loaded with SimpleBlePeripheral, advertise by pressing right button. After this, press the "go" button on HCITester to run the script.
Script Listing
Sctipt
ClearTrace
Send_HCI_Reset
sleep (2000)
#init
Send_GAP_DeviceInit 8, 3, 0, 0, 1
Wait_HCI_Vendor_Specific_Event 5000, 0x67f, , ,
Wait_HCI_Vendor_Specific_Event 5000, 0x600, , , , , ,
#scan for 5 seconds
Send_GAP_SetParam 2, 10000
Wait_HCI_Vendor_Specific_Event 5000, 0x67f, , ,
#start scan
Send_GAP_DeviceDiscoveryRequest 0x03, 0x00, 0
#wait for scan to complete
OnEventWait_HCI_Vendor_Specific_Event 10000, 0x601, ,
OnTimeout
ClearTimeout
OnMismatch
ClearMismatch
RestartEvent
End Event
WaitForAllEvents 12000, True
ClearAllEvents
#establish link
Send_GAP_EstablishLinkReq 0, 0, 0, "3C:2D:B7:84:0D:A5"
Wait_HCI_Vendor_Specific_Event 5000, 0x67f, , ,
Wait_HCI_Vendor_Specific_Event 10000, 0x605, , , , , , , ,
#pair
Send_GAP_Authenticate 0, 0x03, 0, "4d:9f:88:5a:6e:03:12:fe:00:00:00:00:00:00:00:00", 0x00, 16, 63, 0, 0x03, 0, 0x00, 16, 63
Wait_HCI_Vendor_Specific_Event 10000, 0x67f, , ,
Wait_HCI_Vendor_Specific_Event 10000, 0x60a, , , , , , , , , , , , , , , , , , ,
#linkParamUpdate
Wait_HCI_Vendor_Specific_Event 10000, 0x607, , , , ,
Log File
13:27:21.257 --
13:27:21.257 Packet "GAP_DeviceInit", Opcode 0xfe00
13:27:21.257 Parameters:
13:27:21.257 | profileRole : 8 (GAP_PROFILE_CENTRAL)
13:27:21.257 | maxScanResponses : 3
13:27:21.257 | IRK : "0"
13:27:21.257 | CSRK : "0"
13:27:21.257 | signCounter : 1
13:27:21.257 --
13:27:21.257 Outgoing Dump:
13:27:21.257 0000: 01 00 fe 26 08 03 00 00 00 00 00 00 00 00 00 00 ...&............
13:27:21.257 0010: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
13:27:21.257 0020: 00 00 00 00 00 00 01 00 00 00 ..........
13:27:21.261 Incoming Dump:
13:27:21.261 0000: 04 ff 06 7f 06 00 00 fe 00 .........
13:27:21.288 --
13:27:21.288 Packet "HCI_Vendor_Specific_Event", Opcode 0x00ff
13:27:21.306 Parameters:
13:27:21.306 | Event Opcode : 0x067f (CommandStatus)
13:27:21.306 | Status : 0x00 (SUCCESS)
13:27:21.306 | opCode : 0xfe00 (GAP_DeviceInit)
13:27:21.306 | dataLen : 0x00
13:27:21.306 --
13:27:21.320 Incoming Dump:
13:27:21.320 0000: 04 ff 2c 00 06 00 07 7e 70 e5 c5 78 1b 00 04 15 ..,....~p..x....
13:27:21.320 0010: ce 86 0f 2b 63 f9 5d 50 c2 32 bf ec 94 f5 4e d8 ...+c.]P.2....N.
13:27:21.320 0020: 21 aa 99 d1 3e 7a 5c a8 62 f1 bd c0 04 ef 93 !...>z\.b......
13:27:21.335 --
13:27:21.335 Packet "HCI_Vendor_Specific_Event", Opcode 0x00ff
13:27:21.351 Parameters:
13:27:21.351 | Event Opcode : 0x0600 (GAP_DeviceInitDone)
13:27:21.351 | Status : 0x00 (SUCCESS)
13:27:21.351 | devAddr : "78:C5:E5:70:7E:07"
13:27:21.351 | dataPktLen : 0x001b
13:27:21.351 | numDataPkts : 0x04
13:27:21.351 | IRK : "15:CE:86:0F:2B:63:F9:5D:50:C2:32:BF:EC:94:F5:4E"
13:27:21.351 | CSRK : "D8:21:AA:99:D1:3E:7A:5C:A8:62:F1:BD:C0:04:EF:93"
13:27:21.351 --
13:27:21.365 --
13:27:21.365 Packet "GAP_SetParam", Opcode 0xfe30
13:27:21.365 Parameters:
13:27:21.365 | paramID : 2 (TGAP_GEN_DISC_SCAN)
13:27:21.365 | paramValue : 10000
13:27:21.365 --
13:27:21.365 Outgoing Dump:
13:27:21.365 0000: 01 30 fe 03 02 10 27 .0....'
13:27:21.367 Incoming Dump:
13:27:21.367 0000: 04 ff 06 7f 06 00 30 fe 00 ......0..
13:27:21.384 --
13:27:21.384 Packet "HCI_Vendor_Specific_Event", Opcode 0x00ff
13:27:21.399 Parameters:
13:27:21.399 | Event Opcode : 0x067f (CommandStatus)
13:27:21.399 | Status : 0x00 (SUCCESS)
13:27:21.399 | opCode : 0xfe30 (GAP_SetParam)
13:27:21.399 | dataLen : 0x00
13:27:21.399 --
13:27:21.410 --
13:27:21.410 Packet "GAP_DeviceDiscoveryRequest", Opcode 0xfe04
13:27:21.410 Parameters:
13:27:21.410 | mode : 0x03 (DEVDISC_MODE_ALL)
13:27:21.410 | activeScan : 0x00 (Disabled)
13:27:21.410 | whiteList : 0 (Disabled)
13:27:21.411 --
13:27:21.411 Outgoing Dump:
13:27:21.411 0000: 01 04 fe 03 03 00 00 .......
13:27:21.415 Incoming Dump:
13:27:21.415 0000: 04 ff 06 7f 06 00 04 fe 00 .........
13:27:21.429 --
13:27:21.430 Packet "HCI_Vendor_Specific_Event", Opcode 0x00ff
13:27:21.443 Parameters:
13:27:21.443 | Event Opcode : 0x067f (CommandStatus)
13:27:21.443 | Status : 0x00 (SUCCESS)
13:27:21.443 | opCode : 0xfe04 (GAP_DeviceDiscoveryRequest)
13:27:21.443 | dataLen : 0x00
13:27:21.443 --
13:27:21.576 Incoming Dump:
13:27:21.577 0000: 04 ff 14 0d 06 00 00 00 6b d6 e3 14 33 88 bb 07 ........k...3...
13:27:21.577 0010: 02 01 06 03 02 f0 ff .......
13:27:21.600 --
13:27:21.600 Packet "HCI_Vendor_Specific_Event", Opcode 0x00ff
13:27:21.610 Parameters:
13:27:21.610 | Event Opcode : 0x060d (GAP_DeviceInformation)
13:27:21.610 | Status : 0x00 (SUCCESS)
13:27:21.610 | eventTypes : 0x00 (GAP_ADRPT_ADV_IND - Connectable undirected)
13:27:21.610 | addrType : 0x00 (ADDRTYPE_PUBLIC)
13:27:21.610 | addr : "88:33:14:E3:D6:6B"
13:27:21.610 | rssi : -69
13:27:21.610 | dataLen : 0x07
13:27:21.610 | dataField : "02:01:06:03:02:F0:FF"
13:27:21.610 --
13:27:24.016 Incoming Dump:
13:27:24.016 0000: 04 ff 14 0d 06 00 00 00 a5 0d 84 b7 2d 3c d5 07 ............-<..
13:27:24.016 0010: 02 01 06 03 02 f0 ff .......
13:27:24.042 --
13:27:24.042 Packet "HCI_Vendor_Specific_Event", Opcode 0x00ff
13:27:24.063 Parameters:
13:27:24.063 | Event Opcode : 0x060d (GAP_DeviceInformation)
13:27:24.063 | Status : 0x00 (SUCCESS)
13:27:24.063 | eventTypes : 0x00 (GAP_ADRPT_ADV_IND - Connectable undirected)
13:27:24.063 | addrType : 0x00 (ADDRTYPE_PUBLIC)
13:27:24.063 | addr : "3C:2D:B7:84:0D:A5"
13:27:24.063 | rssi : -43
13:27:24.063 | dataLen : 0x07
13:27:24.063 | dataField : "02:01:06:03:02:F0:FF"
13:27:24.063 --
13:27:28.602 Incoming Dump:
13:27:28.602 0000: 04 ff 28 0d 06 00 00 01 de bc 22 2d 9f c7 a7 1b ..(......."-....
13:27:28.602 0010: 02 01 06 11 06 ba 56 89 a6 fa bf a2 bd 01 46 7d ......V.......F}
13:27:28.602 0020: 6e 56 63 ab ad 05 16 0a 18 08 04 nVc........
13:27:28.612 --
13:27:28.612 Packet "HCI_Vendor_Specific_Event", Opcode 0x00ff
13:27:28.627 Parameters:
13:27:28.627 | Event Opcode : 0x060d (GAP_DeviceInformation)
13:27:28.627 | Status : 0x00 (SUCCESS)
13:27:28.627 | eventTypes : 0x00 (GAP_ADRPT_ADV_IND - Connectable undirected)
13:27:28.627 | addrType : 0x01 (ADDRTYPE_STATIC)
13:27:28.627 | addr : "C7:9F:2D:22:BC:DE"
13:27:28.627 | rssi : -89
13:27:28.627 | dataLen : 0x1b
13:27:28.627 | dataField : "02:01:06:11:06:BA:56:89:A6:FA:BF:A2:BD:01:46:7D:6E:56:63:AB:AD:05:16:0A:18:08:04"
13:27:28.627 --
13:27:31.415 Incoming Dump:
13:27:31.415 0000: 04 ff 1c 01 06 00 03 00 00 6b d6 e3 14 33 88 00 .........k...3..
13:27:31.415 0010: 00 a5 0d 84 b7 2d 3c 00 01 de bc 22 2d 9f c7 .....-<...."-..
13:27:31.425 --
13:27:31.425 Packet "HCI_Vendor_Specific_Event", Opcode 0x00ff
13:27:31.434 Parameters:
13:27:31.434 | Event Opcode : 0x0601 (GAP_DeviceDiscovery)
13:27:31.434 | Status : 0x00 (SUCCESS)
13:27:31.434 | numDevs : 0x03
13:27:31.434 | eventType : 0x00 (GAP_ADRPT_ADV_IND - Connectable undirected)
13:27:31.434 | addrType : 0x00 (ADDRTYPE_PUBLIC)
13:27:31.434 | addr : "88:33:14:E3:D6:6B"
13:27:31.434 | eventType : 0x00 (GAP_ADRPT_ADV_IND - Connectable undirected)
13:27:31.434 | addrType : 0x00 (ADDRTYPE_PUBLIC)
13:27:31.434 | addr : "3C:2D:B7:84:0D:A5"
13:27:31.434 | eventType : 0x00 (GAP_ADRPT_ADV_IND - Connectable undirected)
13:27:31.434 | addrType : 0x01 (ADDRTYPE_STATIC)
13:27:31.434 | addr : "C7:9F:2D:22:BC:DE"
13:27:31.434 --
13:27:31.444 --
13:27:31.444 Packet "GAP_EstablishLinkReq", Opcode 0xfe09
13:27:31.445 Parameters:
13:27:31.445 | highDutyCycle : 0 (Disabled)
13:27:31.445 | whiteList : 0 (Disabled)
13:27:31.445 | addrTypePeer : 0 (ADDRTYPE_PUBLIC)
13:27:31.445 | peerAddr : "3C:2D:B7:84:0D:A5"
13:27:31.445 --
13:27:31.445 Outgoing Dump:
13:27:31.445 0000: 01 09 fe 09 00 00 00 a5 0d 84 b7 2d 3c ...........-<
13:27:31.451 Incoming Dump:
13:27:31.451 0000: 04 ff 06 7f 06 00 09 fe 00 .........
13:27:31.463 --
13:27:31.464 Packet "HCI_Vendor_Specific_Event", Opcode 0x00ff
13:27:31.476 Parameters:
13:27:31.476 | Event Opcode : 0x067f (CommandStatus)
13:27:31.476 | Status : 0x00 (SUCCESS)
13:27:31.476 | opCode : 0xfe09 (GAP_EstablishLinkReq)
13:27:31.476 | dataLen : 0x00
13:27:31.476 --
13:27:31.614 Incoming Dump:
13:27:31.614 0000: 04 ff 13 05 06 00 00 a5 0d 84 b7 2d 3c 00 00 50 ...........-<..P
13:27:31.614 0010: 00 00 00 d0 07 00 ......
13:27:31.624 --
13:27:31.624 Packet "HCI_Vendor_Specific_Event", Opcode 0x00ff
13:27:31.634 Parameters:
13:27:31.633 | Event Opcode : 0x0605 (GAP_LinkEstablished)
13:27:31.634 | Status : 0x00 (SUCCESS)
13:27:31.634 | Device Address Type : 0x00 (ADDRTYPE_PUBLIC)
13:27:31.634 | Device Address : "3C:2D:B7:84:0D:A5"
13:27:31.634 | connectionHandle : 0x0000
13:27:31.634 | connInterval : 0x0050
13:27:31.634 | connLatency : 0x0000
13:27:31.634 | connTimeout : 0x07d0
13:27:31.634 | clockAccuracy : 0x00
13:27:31.634 --
13:27:31.643 --
13:27:31.643 Packet "GAP_Authenticate", Opcode 0xfe0b
13:27:31.644 Parameters:
13:27:31.643 | connectionHandle : 0
13:27:31.643 | secReq.ioCaps : 0x03 (NoInputNoOutput)
13:27:31.643 | secReq.oobAvailable : 0 (Disabled)
13:27:31.644 | secReq.oob : "4d:9f:88:5a:6e:03:12:fe:00:00:00:00:00:00:00:00"
13:27:31.644 | secReq.authReq : 0x00
13:27:31.644 | secReq.maxEncKeySize : 16
13:27:31.644 | secReq.keyDist : 63 (sEncKey|sIdKey|sSign|mEncKey|mIdKey|mSign)
13:27:31.644 | pairReq.Enable : 0 (Disabled)
13:27:31.644 | pairReq.ioCaps : 0x03 (NoInputNoOutput)
13:27:31.644 | pairReq.oobDataFlag : 0 (Disabled)
13:27:31.644 | pairReq.authReq : 0x00
13:27:31.644 | pairReq.maxEncKeySize : 16
13:27:31.644 | pairReq.keyDist : 63 (sEncKey|sIdKey|sSign|mEncKey|mIdKey|mSign)
13:27:31.644 --
13:27:31.644 Outgoing Dump:
13:27:31.644 0000: 01 0b fe 1d 00 00 03 00 4d 9f 88 5a 6e 03 12 fe ........M..Zn...
13:27:31.644 0010: 00 00 00 00 00 00 00 00 00 10 3f 00 03 00 00 10 ..........?.....
13:27:31.644 0020: 3f ?
13:27:31.647 Incoming Dump:
13:27:31.647 0000: 04 ff 06 7f 06 00 0b fe 00 .........
13:27:31.658 --
13:27:31.658 Packet "HCI_Vendor_Specific_Event", Opcode 0x00ff
13:27:31.667 Parameters:
13:27:31.667 | Event Opcode : 0x067f (CommandStatus)
13:27:31.667 | Status : 0x00 (SUCCESS)
13:27:31.667 | opCode : 0xfe0b (GAP_Authenticate)
13:27:31.667 | dataLen : 0x00
13:27:31.667 --
13:27:33.922 Incoming Dump:
13:27:33.922 0000: 04 ff 6a 0a 06 00 00 00 00 01 10 ce e8 5c d6 d1 ..j..........\..
13:27:33.922 0010: 39 59 df e1 79 86 0b 28 60 2a 9e 5d fa e3 81 56 9Y..y..(`*.]...V
13:27:33.922 0020: c8 a1 7c 62 7b 01 10 13 c2 a5 8c 62 78 de 2b b9 ..|b{......bx.+.
13:27:33.922 0030: 5a a7 71 92 3b 0d ef c6 d0 39 5c bf 51 d7 31 69 Z.q.;....9\.Q.1i
13:27:33.922 0040: 9f 01 8f 17 18 25 65 8a 6e 68 de 2e 89 1a f8 a5 .....%e.nh......
13:27:33.922 0050: a3 82 a5 0d 84 b7 2d 3c 01 43 07 44 f0 94 33 ad ......-<.C.D..3.
13:27:33.922 0060: 6f e2 7e 36 4b af 94 32 bd ff ff ff ff o.~6K..2.....
13:27:33.940 --
13:27:33.940 Packet "HCI_Vendor_Specific_Event", Opcode 0x00ff
13:27:33.952 Parameters:
13:27:33.952 | Event Opcode : 0x060a (GAP_AuthenticationComplete)
13:27:33.952 | Status : 0x00 (SUCCESS)
13:27:33.952 | connectionHandle : 0x0000
13:27:33.952 | authState : 0x00
13:27:33.952 | securityInfo : 0x01 (Enabled)
13:27:33.952 | securityInfo.LTKsize : 0x10
13:27:33.952 | securityInfo.LTK : "CE:E8:5C:D6:D1:39:59:DF:E1:79:86:0B:28:60:2A:9E"
13:27:33.952 | securityInfo.DIV : 0xfa5d
13:27:33.952 | securityInfo.rand : "E3:81:56:C8:A1:7C:62:7B"
13:27:33.952 | devSecInfo : 0x01 (Enabled)
13:27:33.952 | devSecInfo.LTKsize : 0x10
13:27:33.952 | devSecInfo.LTK : "13:C2:A5:8C:62:78:DE:2B:B9:5A:A7:71:92:3B:0D:EF"
13:27:33.952 | devSecInfo.DIV : 0xd0c6
13:27:33.952 | devSecInfo.rand : "39:5C:BF:51:D7:31:69:9F"
13:27:33.952 | identityInfo : 0x01 (Enabled)
13:27:33.952 | identityInfo.IRK : "8F:17:18:25:65:8A:6E:68:DE:2E:89:1A:F8:A5:A3:82"
13:27:33.952 | identityInfo.BD_ADDR : "3C:2D:B7:84:0D:A5"
13:27:33.952 | signingInfo : 0x01 (Enabled)
13:27:33.952 | signingInfo.CSRK : "43:07:44:F0:94:33:AD:6F:E2:7E:36:4B:AF:94:32:BD"
13:27:33.952 | signingInfo.signCounter : 0xffffffff
13:27:33.952 --
13:27:38.334 Incoming Dump:
13:27:38.334 0000: 04 ff 0b 07 06 00 00 00 20 03 00 00 e8 03 ........ .....
13:27:38.344 --
13:27:38.344 Packet "HCI_Vendor_Specific_Event", Opcode 0x00ff
13:27:38.353 Parameters:
13:27:38.353 | Event Opcode : 0x0607 (GAP_LinkParamUpdate)
13:27:38.353 | Status : 0x00 (Success)
13:27:38.353 | connectionHandle : 0x0000
13:27:38.353 | connInterval : 0x0320
13:27:38.353 | connLatency : 0x0000
13:27:38.353 | connTimeout : 0x03e8
13:27:38.353 --
13:27:38.366 --
13:27:38.366 *** Script End ***
13:27:38.366 --