Hello,
I am using the LP-CC2652RB in an application where I need to power the LaunchPad externally (not through USB). Would the TPS7A1633DGNR LDO work? This has a maximum of 100mA load current. I am using the CC2652R1 as a peripheral device that is derived from the "Simple Peripheral" profile.
In addition to the steady state DC load current of the CC2652R1- are there any significant inrush currents associated with power on?