1.A25 pin:SLOW_ CLK_ IN, Must give a 32.768KHz clock signal? Is it OK set to no connect ?
2. A6 pin: how to connect nSHUTD? Pull directly up to VDD_1.8V is OK?
3.MCU and Bluetooth are connected by UART four signals. Do we need special command to realize communication?
4.Is the following circuit diagram OK(R100 NC)?