I need to save data in non volatile memory.
It seems that I need to use the HalFlashWrite and HalFlashRead functions.
My questions are regarding flash page number and offset of the read method.
How to get those value?
Why flash number and offset are not required for the HalFlashWrite function ?
In my example bellow, I try to write 6 bytes to address 0X2A80, what are the page and offset I need to use in the HalFlashRead function ?
//to write
uint8 temp[6] = {0x61,0x62,0x63,0x64,0x65,0x66};
HalFlashWrite(0x2A80,temp ,2);
//to read
uint8 readBuffer[8];
HalFlashRead(?, ?, readBuffer, 2);