Other Parts Discussed in Thread: CC2640, CC2540
I have put the HIDEmuKbd exp for the CC2640 on the SensorTag where I leave only 2 buttons and make a new map for it.
Now I want to example how it work. I have also CC2540 DOngle and CC Debugger:
The questions are as follow:
1. If I want to use the Dongle as a peer device and make the advertising and also see all the traffic between them- What FW shell I put over the CC2540 Dongle, and which PC software will allow me to take in charge over the HIDApp (scan, notification enable ect) ad also see what the HIDApp send?
2. Where can I find the FW and the PC application in TI sit for doing so?
3. Is there a good user guide for the HIDEmuKbd application so I can know which handle is the notification and the battery service (Table show all the characteristic of the App),so I can allow those services from the PC application?
Thanks Bar.