Hi, I am using CC2640R2F in one of my circuit design. FYI, the UART_TX and UART_RX of my CC2640R2F is connected to the UART_RX and UART_TX of an MCU. When I tried to launch the BTool (with the correct COM port setting and the use of level shifter board), I got the following error message:
GAP Device Initialization Timeout.
Device May Not Function Properly.
Also, I notice that the current drops from 25 mA to 9 mA (at 3.3V) when I launched BTool. I assume 25 mA is the total current needed to power both CC2640R2F and the MCU.
Please advise.
Thanks.
Best Regards,
Zhi Wei