Other Parts Discussed in Thread: CC2520, CC2652R
Hi I am using ZigBee device store.ncd.io/.../ which consist of IC CC2520 using UART pin for RX and TX and VCC 3.3v Pin and ground pin and I want to send the data from Zigbee device BLE module www.rhydolabz.com/.../low-energy-bluetooth-40-moduledbm01-p-1483.html with IC CC2540 and test it, I am looking for possible circuit connection to send the data from ZigBee to BLE module possible , Also need to know for making these kind of connection, do I have to use any ADC IC for data conversion or not ?
Note: Both the devices are connected by USB electric shield to laptop