Part Number: CC2640
Greetings,
I have CC2640 programmed with HostTest app based on TI BLE SDK ver.2.2.2. In my experiment the chip works as central and communicates with Android phone that works as peripheral . During communication they negotiated to use MTU size up to 203 bytes and then my chip sends 200 bytes notifications as fast as possible. After each notification I checks status in Command Status event to ensure the transfer to the chip was successfully completed.
Sometimes after notification the chip responses with Hardware Error event (0x04 0x10 0x01 0x81) and after that responses with Command Status that has 0x04 status. In this situation I repeats notification and it successfully received by Android phone.
So my question is could anybody explain why this Hardware Error event appears and is it safe to proceed with notifications without RF-chip reset and re-initialization?
May it is safe only if value exactly 0x81?
Thank you in advance,
Sergiy.