This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2650EM-7ID-RD: Connecting CC2650 with PC over uart using FTDI

Part Number: CC2650EM-7ID-RD

Hello,

I'm trying to set up a UART connection between a CC265DK_7ID and my PC.

I'm using a FT232RL from FTDI for the USB_UART conversion and connected the RX/TX (RX: RF1.7 and TX: RF1.9)of the FT232 with those of the CC2650 (as well as GND and VCC ), I also have the SmartRF06 EB, I have tested my program using the EB and I can see my data printed out over uart. However, I faild to establish the uart connexion using the FTDI

I wonder where is the problem?

Best regards.