This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2564MODA: CC2564MODA

Part Number: CC2564MODA
Other Parts Discussed in Thread: CC2564C, CC2564

Hi,

I want to develop a bluetooth speaker system with the following features.

- Stereo audio output.

- Connecting with Android or Iphone via bluetooth.

- Playing music with AUX output on any device.

- Playing the music in the USB device.

Which product or development kit can I use for a device with these features?

For example, when I examine your site, I think I can solve the bluetooth issue with CC256X series integrations.

We are waiting for your suggestions.Thank You.

  • Yes, you are correct, the dual mode BT devices based on CC2564 will provide the needed support for streaming audio via A2DP.  We will recommended the latest revision of the chip CC2564C which was recently certified component BT 5.1.  I'd suggest you start looking here:

    https://www.ti.com/product/CC2564C

    There are links to the available EVM that can work with TI Sitara LInux based EVMs, or with TI's MSP432 launchpad or STM32 EVM depending on your host choice.

    Regards,

    Travis