This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2564MODN: Bluetooth Stack for CC2564 interface with MSP430F6779

Part Number: CC2564MODN
Other Parts Discussed in Thread: MSP430F6779, CC2564, MSP430F6779A,

I am interfacing CC2564MODn with MSP430F6779 micro-controller.
I have following questions.
1. Which bluetooth stack do I need to use?
Online I saw Bluetopia stack. Is this the official one that TI recommends?
If so do you provide source code for the same? 
2. Any other open source library that TI would recommend for CC2564 chip?
3. Is there a development board or evaluation kit that can be used for quick prototype and testing?
4. If I understand correct CC2564 code cannot be flashed but the stack resides in MSP430(Host) chip?

Thanks