Part Number: BOOSTXL-AOA
Greetings,
As I upgrade the SDK from 3.40 to newest version 4.40, now I can get raw IQ both from master and passive node, and they match the frame structure well. I notice the default aoa_params also changes: now the aoa_slot_duration =2 and aoa_sampling_control is int(‘0x11’,16), which I assume there is antenna switching. But I did not see any antenna idx change in any .csv files, the idx is always 1.
How can we enable antenna switching, and we can see antenna idx changes in the .csv file. Clément
Btw, what does the idx 1 or 2 in .csv file, does it mean antenna 1-1 and 1-2( 2nd array of 1st row ULA), or it simply mean 1st ULA and 2nd ULA ?
Best.
Jet