Other Parts Discussed in Thread: CC2650,
Hello,
I am porting a code written for cc2640r2 to cc2640f128.
This code does not use bluetooth. It uses only the following functions:
-ADC;
-PWM;
-Timer;
-Watchdog;
-NVS.
As there is no sdk for cc2640f128, I used "tirtos_cc13xx_cc26xx_2_21_01_08" with the example "empty".
In this example it was possible to compile and program cc2640f128.
The problem is that when adding NVS to the code the following error message is displayed:
"
unresolved symbol NVS_config, first referenced in C: /ti/tirtos_cc13xx_cc26xx_2_21_00_06/products/tidrivers_cc13xx_cc26xx_2_21_00_04/packages/ti/drivers/lib/drivers_cc26xxware.aem3 <NVS.oemf ++ C8 / kek_r
"
The code used in the cc2640r2 that works uses the following functions:
NVS_init ();
NVS_Params nvsParams;
NVS_Params_init (& nvsParams);
nvsHandle = NVS_open (0, & nvsParams);
NVS_getAttrs (nvsHandle, & regionAttrs);
Are there any examples of using NVS for this processor or some other SDK compatible with it?