Hi,
I recently used the custom Bluetooth Service Generator at Simplelink Academy CC2640R2F SDKv4.40. Why is the size of len uint16_t, at earlier versions this was uint8_t..
extern bStatus_t XXXXservice_SetParameter(uint8_t param, uint16_t len, void *value); extern bStatus_t XXXXservice_GetParameter(uint8_t param, uint16_t *len, void *value) typedef void (*xxxxserviceChange_t)(uint16_t connHandle, uint16_t svcUuid, uint8_t paramID, uint16_t len, uint8_t *pValue);
-kel