This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

about CC2564 muRata LBMA1BGUG2 F/W not work on Linux kernel 3.10

Other Parts Discussed in Thread: CC2564

Hi Ti supporter.

PLCM use muRata LBMA1BGUG2 on VVX600 product. This product had GA.

VVX600 use BRCM chip +  Linux kernel 2.6 + muRata LBMA1BGUG2 + F/W (51K size, release 04-Apr-2012 ) + bluez 4.48.

 

Now PLCM update this product to VVX601.

VVX601 use BRCM chip + Linux kernel 3.10.77 + muRata LBMA1BGUG2 + F/W (51K size, release 04-Apr-2012 ) + bluez 4.48(or 4.101).

 

The F/W(51K size, release 04-Apr-2012 )  can’t work with Linux kernel 3.10.77.

 

We can get some info form F/W.

Description : Trio Orca 5500 L ROM Initialization Script

Compatibility: Trio/Orca/5500, 6.0.15 ROM

Last Updated: 04-Apr-2012   8:23:20.77

Version     : TI_P6_15.59

Notes       : Use this script on Trio, Orca or 5500, 6.0.15 ROM device only (FW v6.0.15)

Polycom customization en

Failed log:

-bash-3.2#  hciattach -s 115200 ttyS1 texas

Found a Texas Instruments' chip!

Firmware file : /lib/firmware/TIInit_6.6.15.bts

Loaded BTS script version 1

[  287.360000] Bluetooth: Unknown HCI packet type fe

[  289.360000] Bluetooth: hci0 command 0x1003 tx timeout

[  291.360000] Bluetooth: hci0 command 0x1001 tx timeout

[  293.360000] Bluetooth: hci0 command 0x1009 tx timeout

Initialization timed out.

Please update this F/W ‘TIInit_6.6.15_old.bts’, make it work on Linux kernel 3.10.

Waye