Texas Instruments, Inc.

SmartRF Flash programmer  Release Notes

-------------------------------------------------------------------------------
-------------------------------------------------------------------------------

-------------------------------------------------------------------------------
N O T E!
To ensure that everything is cleaned up from the startup menu, it is 
recommended to uninstall the old version before installing the new version.
-------------------------------------------------------------------------------
Version 1.12.3.0 January 5. 2012 
-------------------------------------------------------------------------------
- MSP430.dll updated to version 3.2.1.9. This is a major update and to 
  downgrade back to version 2.x it is required with a manual procedure.
  See http://www.ti.com/mspds for more details. 
-------------------------------------------------------------------------------
Version 1.12.2.0 October 27. 2011 
-------------------------------------------------------------------------------
- Problem with programming of the Tetst Boards used in Lab solved. 
-------------------------------------------------------------------------------
Version 1.12.1.0 October 10. 2011 
-------------------------------------------------------------------------------
- Problem with programming of IEEE address for devices with flash size of 32 kB 
  or less solved.
-------------------------------------------------------------------------------
Version 1.11.1.0 April 06. 2011 
-------------------------------------------------------------------------------
- Problem with application window not visible at startup solved.");
- Potential problem with reading of IEEE address for devices with 32kB or less 
  Flash solved.
- Warning about \"Unknown FW id\" will only appear ones.
- Problem that the dialog to view info page was opened with a mouse click 
  outside the dedicated button solved.
-------------------------------------------------------------------------------
Version 1.11.0.0 Beta February 18. 2011 
-------------------------------------------------------------------------------
- Console programmer: Support for programming without erase and without verify.
- Console programmer: Support for programming without erase but with verify of CRC.
-------------------------------------------------------------------------------
Version 1.10.2.0 Beta December 08. 2010 
-------------------------------------------------------------------------------
- This version includes the signed USB drivers. This means it can be used on 
  64 bit Windows Operating systems. 
- New feature to automatically update the firmware of Evaluation Boards added.
- New feature to erase flash is added.
- "Retain IEEE Address" will be on by default on startup.
- A warning is given if trying to program firmware on 04EB with SoC connected.  
-------------------------------------------------------------------------------
Version 1.10.0.0 Beta October 20. 2010 
-------------------------------------------------------------------------------
- This version is built with a new version of the Cebal library. The new
  Cebal library is based on the updated USB Driver from Thesycon. The new
  driver file is called "Cebal2".
- Problem with programming of any MSP430 device connected via MSP-FET430UIF solved.
- The layout of the tabs has been changed to make the difference between programming 
  of the SoCs and the EBs more intuitive for the user.
- The CLI version now support setting of the lock bits for CC253x and CC254x.

Known issues:
  Evaluation Boards previously used on the PC will not appear in the list of
  connected devices. This is because of a problem with the new USB library.
  To solve this, it is necessary to do an update of the driver. This can be
  done from the Device Manager in Windows.
  1. Open Device Manager From the Start->Control panel->System". Select the
     "Hardware" tab and click on the "Device Manager" button.
  2. The device should be listed under "Cebal controlled devices". 
     Right click on the device and select "Update driver...". The driver should
     be updated. Right click on the device and select "Properties". Select the
     "Driver" tab and verify that the Driver version is 2.50.0.0   
-------------------------------------------------------------------------------
Version 1.9.0.1 September 29. 2010 
-------------------------------------------------------------------------------
- Console programmer supporting CC2540 with 6 byte IEEE MAC address.
- Console programmer supporting reading of both primary and secondary IEEE addr.
-------------------------------------------------------------------------------
Version 1.9.0.0 September 28. 2010 
-------------------------------------------------------------------------------
- Support for programming of 48 bit MAC address for CC2540 added.
- Support for 8 digits number for device ID when programming bootloader for
  SmartRF05EB and CC Debugger.
- After programming of MSP430 devices the \"Verify against hex file\" action
  was enabled. This action is not implemented and should therefore not be enabled.
- Increment of Board identification (Device ID) when programming the bootloader.    
-------------------------------------------------------------------------------
Version 1.8.1.0 June 22. 2010 
-------------------------------------------------------------------------------
- Fixed problem with error message if enumeration of MSP430 device failed.
-------------------------------------------------------------------------------
Version 1.8.0.0 June 13. 2010 
-------------------------------------------------------------------------------
- Console programmer supporting patching of encryption keys before programming
  of hex file. 
- Console programmer supporting flash verification by checking the CRC of each 
  page instead of read back of every byte.
- Version numbering added to the console programmer (1.8.l).
- Compiler changed from VC++ 6.0 to VC++ 2005.   
- MSP430.dll updated to version 2.4.4.0
-------------------------------------------------------------------------------
Version 1.7.1.0 January 20. 2010 
-------------------------------------------------------------------------------
- Fixed problem with CC2533 flash size detection
- Fixed bug relating to incorrect message of "debug interface lock" when 
  attempting EPV of a chip with debug interface lock (the debug interface lock 
  is now removed after Erase operation, so there is no longer necessary to 
  attempt twice).
- Descriptive error message added when attempting to program a HEX image with 
  data at addresses exceeding the chip's flash size (earlier only "flash 
  programming failed" was reported).
- Increased max number of connected EBs supported from 32 to 64. 
- Fixed bug relating to warning/request of firmware upgrade on MSP430 Debug 
  tool when doing SoC/EB actions. The fix will only display this warning if 
  the MSP430 tab is shown.
- Filtering on not supported devices improved in SoC device list.  
- MSP430.dll updated to version 2.4.2.0
-------------------------------------------------------------------------------
Version 1.7.0.0 January 05. 2010 
-------------------------------------------------------------------------------
- Added support for CC2533
- Consol programmer now supporting read/write IEEE address for CC2530/CC2533
- SmartRF04 EB Firmware upgrade: Revision 0042
- SmartRF05 EB Firmware upgrade: Revision 0012
- CC Debugger Firmware upgrade: Revision 0012
-------------------------------------------------------------------------------
Version 1.6.2.2 April 30. 2009 
-------------------------------------------------------------------------------
- Fixed problem with programming of lock bits for bootloader and page lock
  for CC243x, CC251x and CC111x
-------------------------------------------------------------------------------
Version 1.6.1.0 April 24. 2009 
-------------------------------------------------------------------------------
- Added support for CC-Debugger
- Added support for programming of CC2530 and CC2531.
- Updated version of msp430.dll (2.4.0.0) to support CC430.
- A button to refresh the list of connected MSP430 devices has been added.
-------------------------------------------------------------------------------
Version 1.5.5.0 December 12. 2008 
-------------------------------------------------------------------------------
- Fixed problem with not giving an error message if "Retain IEEE" used on a
  chip with debug interface is locked.
-------------------------------------------------------------------------------
Version 1.5.4.0 November 20. 2008 (Beta) 
-------------------------------------------------------------------------------
- Include a fix to enable programming of bootloader on 05EB from another 05EB board
-------------------------------------------------------------------------------
Version 1.5.3.0 October 28. 2008 (Beta)
-------------------------------------------------------------------------------
- Support for reading information page if applicable.
-------------------------------------------------------------------------------
Version 1.5.2.0 October 28. 2008 (Beta)
-------------------------------------------------------------------------------
- Support for programming of 05 Temp board added. 
- Problem with overlapping input fields on GUI fixed.
- Version 2.3.5.0 of the msp430.dll
-------------------------------------------------------------------------------
Version 1.5.1.0 July 7. 2008 (Beta)
-------------------------------------------------------------------------------
- Support for programming of more devices