Other Parts Discussed in Thread: TRF7970A
Hi Team,
My customer is detecting the presence of passive cards with the TRF7970A without the need for additional hardware. They are using the Linux NFC Subsystem with the provided NFC trf7970a.c drive and a boostpack DLP-7970AB.
According to https://www.ti.com/lit/an/sloa184/sloa184.pdf , an RSSI detection loop is the only solution that does not require extra hardware. Is this is different from the example polling loop in the reader/writer example on page 14(link)? Or is the RSSI detection implemented in the “Response Received?” block?
The goal is to have the reader in a proximity detection loop, consuming as little power as possible, until a tag is presented and begin sending commands to read from it. I’m trying to determine how this RSSI detection loop will save power compared to normal polling. Is polling the same as the RSSI detection loop?
Looking forward to the discussion!
Best Regards,
Madhurya