Hi Team RF430,
What is the current TI recommendation WRT hardware & software for Production/Manufacturing Testing of the RF430CL330H?
Hardware?
Software?
Command Line & scripting tools?
Any recommended test flow/algorithms?
Thanks, Merril
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team RF430,
What is the current TI recommendation WRT hardware & software for Production/Manufacturing Testing of the RF430CL330H?
Hardware?
Software?
Command Line & scripting tools?
Any recommended test flow/algorithms?
Thanks, Merril
Hi Merril,
we are not providing any hardware or software for a production test of the RF430CL330H. Production tests are up to the customer. The RF430CL330H is a NFC Tag Type 4 compatible device which works according the ISO14443-B standard. If just a simple go/no-go test is needed, any reader compliant to this standard can be used to read the NDEF message from the RF430CL330H.
If also parameters should be checked, then NFC readers like the one provided from i.e. Micropross can be used.
Best Regards,
Helfried